Code Red Broken Source Download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Red Broken Source Download

1,240 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sun Mar 04 23:04:09 MST 2012
The "SourceDownload" page on the Code Red Wiki offers a download for the source of the GNU tool chain and library.

The file claims to be 122 MBytes (what I would expect) but every time I try to download, it stops as 20Mb. [Trying to open the archive fails with CRC errors].

As I have the free version (LPCXpresso) there is no legal way I can email their support to let them know and the don't appear to have a forum of their own.
Their wiki doesn't even have a feed back option.

Can some one with a valid RED Suite licence drop a line to the support guys.

Thanx, Mike
0 Kudos
Reply
3 Replies

1,233 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Mon Mar 05 05:21:26 MST 2012
I still breaks for me (consistently) at 19.7 MB.
The link on the CodeRed page is "http://support.code-red-tech.com/CodeRedWiki/SourceDownloads?action=AttachFile&do=get&target=arm-201..."
I use WinXP Prof SP3, FireFox 3.6.27 add on "Download StatusBar", Avast! Free V7.

Actually, I just want the library and startup source code. Do you have the _exact_ version number so I can find it (e.g.) on SourceForge instead?
Or do you have FTP access?

Regards.
0 Kudos
Reply

1,233 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Mar 05 01:31:09 MST 2012
I have just tried, and it works here.

We have had reports of problems when using Internet Explorer, but using a different browser (Firefox, Chrome, Safari) works. If you must use IE, try clearing all of the caches, download history and cookies, and then try again.
0 Kudos
Reply

1,233 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Mon Mar 05 01:07:23 MST 2012
CodeRed monitors and gives support on this forum so there's a good chance they'll respond here.

A few months ago I was able to download the src successfully.
0 Kudos
Reply