Code Debug LPC1343

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Debug LPC1343

795 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andersonf on Wed May 11 06:33:29 MST 2011
Hello,
I'm starting to tinker with ARM and now rode a board with LPC1343.
I set LPCXpresso and compiled some code.
The board has not ridden it for debug connections in circuit.
I do not have this card X-Link for debugging too, and did not want to debug in real time.
But I want to debug the code I'm producing, check value of the register, verify the values ​​of variables!
I would just debug the code I'm writing?
When asked to debug it says can not find the emulator and abort the operation.
Thanks!
0 Kudos
Reply
1 Reply

782 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed May 11 06:52:31 MST 2011
It's not possible to debug without board and LPC-Link :mad:
This debugger is an 'On-Chip Debugger' and therefore implemented in this chips.
0 Kudos
Reply