Change variable value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change variable value

2,539 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Mar 15 02:43:02 MST 2016
Dear, I have a simple problem that cannot solve.

I have :
- Last version of LPCXpresso v8.1.2 [Build 603] [2016-03-07]
- LPC-Link Probe v1.3
- My board with LP1758

The problem is when, in debug mode in suspen condition, I cannot modify a variable value in Expressions.

What am I doing wrong trivially ??

Thanks

Stefano

0 Kudos
Reply
4 Replies

2,513 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

2,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Mar 16 06:07:50 MST 2016
Thanks, I confirm that the problem is solved !!!   :)  :)  :)
0 Kudos
Reply

2,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Mar 16 01:17:50 MST 2016
LPCXpresso IDE v8.1.4, which we have just released, should resolve this issue.

Regards,
LPCXpresso Support
0 Kudos
Reply

2,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Mar 15 03:46:10 MST 2016
There is an issue with LPCXpresso IDE v8.1.2 where some debugger writes to memory silently fail. We expect to make a new version available with this issue resolved in the next day or so.

Regards,
LPCXpresso Support
0 Kudos
Reply