Can't flash program (Error 53: License)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't flash program (Error 53: License)

1,487 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mondo90 on Sat Aug 23 02:32:29 MST 2014
Hello,
lpc problems continuation ;/ This time my program in debug mode works properly but I can't flash it. When I try to do so I get:
"Error:53: License does not permit flash operations from command line". I click ok and next windows popup with lines:
(..)
Nt: Connected: was_reset=false. was_stopped=true
Cr:f PCXpresso Free License - Download limit is 8K (UNREGISTERED)
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed

Ofcourse, my program is registered and activated, even welcome tab says "LPCXpresso (Free Edition) is fully activated". I have read similar problem thread and there was advice to reactivate product. I did it but with no success, problem still occurs.
PS: if it matters, my *.axf file is located in Debug directory.

What's wrong ?
0 Kudos
Reply
5 Replies

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 25 00:59:36 MST 2014
So, if you read the log, you will notice that ipconfig.exe and cscript.exe are not found. This is most likely due to a PATH problem with your setup. If these cannot be found on your path by the debug driver then it will not work.

Please take the time to read, understand and fix the problem as described in this FAQ.
http://www.lpcware.com/content/faq/lpcxpresso/flash-image-too-large

Note that in this case the output from the redlink console is irrelevant as you are not using an lpc-link2 probe.
0 Kudos
Reply

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mondo90 on Sun Aug 24 05:00:11 MST 2014
I feel like I was very clear about my problem but ok, below are all possible details:

System: Windows 7 (64bit)
IDE:  LPCXpresso v7.3.0 [Build 186] [2014-07-09] || I also have tested on v6 version with no success
Micocontroller: LPC1114
The problem:
When I try to flash program into microcontroller memory I get error:

Quote:
53: License does not permit flash operations from command line


I click OK and then next windows appears:

Quote:


Ni: LPCXpresso Debug Driver v7.3 (Jul  2 2014 14:56:01 - crt_emu_lpc11_13_nxp.exe build 10)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID:  BB11477. Info: HID64HS12
Nc: SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: Loaded LPC11_12_13_4K_1K.cfx: LPC11_12_13 (4K Flash, min 1K RAM) Jul  1 2014 11:50:50  On-chip Flash Memory

Nc: NXP: LPC1114/302  Part ID: 0x00000000
Pc: ( 65) Chip Setup Complete
Nazwa 'ipconfig.exe' nie jest rozpoznawana jako polecenie wewn©trzne lub zewn©trzne,
program wykonywalny lub plik wsadowy.
Nazwa 'cscript.exe' nie jest rozpoznawana jako polecenie wewn©trzne lub zewn©trzne,
program wykonywalny lub plik wsadowy.
Nt: Connected: was_reset=false. was_stopped=true
Cr:f PCXpresso Free License - Download limit is 8K (UNREGISTERED)
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed


Console log:

Quote:
[Started server]
[Connected on port 3025]
redlink>
redlink>
redlink>
redlink>
redlink>
redlink>
redlink>ProbeList
No probes found
redlink>
redlink>
redlink>ProbeList
No probes found
redlink>
redlink>
redlink>
redlink>
redlink>
redlink>
redlink>ProbeList
No probes found
redlink>
redlink>
redlink>ProbeList
No probes found



Program debugs ok and works ok problems start to happen when I click flash icon.
Can you help ?
0 Kudos
Reply

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Aug 23 08:42:23 MST 2014
Please provide some details that might help us identify your problem. For example... Which versions f LPCXpresso? Which operating system and version are you running on? What is the full text of the log? What was all the output from the diagnostics?
0 Kudos
Reply

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mondo90 on Sat Aug 23 03:18:16 MST 2014
Thanks for reply. As I said earlier my program debug correctly, problem occurs when I try to flash program image. Plus there is no information about too large image. Anyway I have tested "cscript hello.vbs" and in my case it works properly.

Any ideas ;/ ?
0 Kudos
Reply

1,431 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Aug 23 02:59:49 MST 2014
In the first place, please see:

http://www.lpcware.com/content/faq/lpcxpresso/flash-image-too-large

Regards,
LPCXpresso Support
0 Kudos
Reply