CODE RED: SWD Connector

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CODE RED: SWD Connector

764件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Nov 08 08:22:54 MST 2012
[FONT=Tahoma][SIZE=1]On your page "[/SIZE][/FONT][FONT=Tahoma][SIZE=1]SWD / JTAG Connectors and Pinout", you recommend a 10K to 100K
pull-down to ground for SWCLK.

Various documents I have seen state that the SWD clock (SWCLK) is idle [I]high[/I].

So is this a mistake on your part, and the clock line is to be pulled [B]up[/B]? :confused:
Or is there something that I still do not understand?

Does this pull-up (or pull-down) apply to both the target board and the SWD adapter?

BTW: The LPCXpresso 1769 uses a tri-stated buffer for SWCLK idle (i.e. pull up)
and has [I]no[/I] pull ups or downs on the target side.

Please will you clarify/confirm the details, including the recommendations for
custom (SWD debugged) target boards.

Cheers, Mike.
[/SIZE][/FONT]
0 件の賞賛
返信
1 返信

741件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Nov 08 11:16:56 MST 2012
http://support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections

AFAIK, though, all NXP Cortex devices have internal pull-ups on both SWCLK and SWDIO. I didn't include them on an LPC1114 board I designed.
0 件の賞賛
返信