CMSISv2p00_LPC17xx adding problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSISv2p00_LPC17xx adding problem

3,754件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by natwar on Wed Mar 13 00:15:59 MST 2013
while creating project I am unable to add "CMSISv2p00_LPC17xx" in "CMSIS library to link project to" option.Please tell me how to add this.
0 件の賞賛
返信
7 返答(返信)

3,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by natwar on Fri Mar 15 04:54:01 MST 2013
[SIZE=4]Thanx to all. I copied [U][B]RDB1768cmsis2_LCDlib [U][B]and[/B][/U] CMSISv2p00_LPC17xx[/B][/U] and now I am able to coding using CIMSIS files.
Thanx again to all.[/SIZE]
0 件の賞賛
返信

3,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Mar 13 05:56:53 MST 2013
The library projects that you are missing are in the same ZIP file that you imported the RDB1768cmsis2_uIP project from. Why don't you just import all of the projects from that ZIP into your workspace  :confused:

Suggest you go back and read the Getting Started again/for the first time. And maybe watch the video...

http://www.youtube.com/watch?v=E6vSPloei-0

HTH!
0 件の賞賛
返信

3,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by natwar on Wed Mar 13 05:24:29 MST 2013
[SIZE=4]Description

Errors:
[B]cannot find -lCMSISv2p00_LPC17xx
cannot find -lRDB1768cmsis2_LCDlib
make: *** [RDB1768cmsis2_uIP.axf] Error 1
[/B]


Warnings:
[B][SIZE=4]Invalid project path: Include path not found (CMSISv2p00_LPC17xx\inc).RDB1768cmsis2_uIPpathentryPath Entry Problem
Invalid project path: Include path not found (RDB1768cmsis2_LCDlib\inc).RDB1768cmsis2_uIPpathentryPath Entry Problem
[SIZE=4][/SIZE][/SIZE][/B][/SIZE]
0 件の賞賛
返信

3,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by natwar on Wed Mar 13 05:21:58 MST 2013
[SIZE=7]Description
[B]
Errors:
cannot find -lCMSISv2p00_LPC17xx
cannot find -lRDB1768cmsis2_LCDlib
make: *** [RDB1768cmsis2_uIP.axf] Error 1[/B]


Warnings:
[B]Invalid project path: Include path not found (CMSISv2p00_LPC17xx\inc).RDB1768cmsis2_uIPpathentryPath Entry Problem
Invalid project path: Include path not found (RDB1768cmsis2_LCDlib\inc).RDB1768cmsis2_uIPpathentryPath Entry Problem[/B]
[/SIZE]
0 件の賞賛
返信

3,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by natwar on Wed Mar 13 05:20:11 MST 2013
I am getting this msg in o/p window.

DescriptionResourcePathLocationType
[B][B]cannot find -lCMSISv2p00_LPC17xx[/B][/B]RDB1768cmsis2_uIP C/C++ Problem
[B]cannot find -lRDB1768cmsis2_LCDlib[/B]RDB1768cmsis2_uIP C/C++ Problem
make: *** [RDB1768cmsis2_uIP.axf] Error 1RDB1768cmsis2_uIP C/C++ Problem
Invalid project path: Include path not found (CMSISv2p00_LPC17xx\inc).RDB1768cmsis2_uIPpathentryPath Entry Problem
Invalid project path: Include path not found (RDB1768cmsis2_LCDlib\inc).RDB1768cmsis2_uIPpathentryPath Entry Problem
0 件の賞賛
返信

3,647件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Wed Mar 13 00:49:15 MST 2013
Why do they still make 'getting started' guides :confused:

Nobody seems to read them anyway
0 件の賞賛
返信

3,646件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Mar 13 00:34:02 MST 2013
Did you even read the message on the dialog. See attached screenshot, and read it.
0 件の賞賛
返信