CMSIS Version 3.20

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CMSIS Version 3.20

1,076 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun May 26 06:08:05 MST 2013
Are there plans to update CMSIS to V3.20 this year? It's including a lot of forgotten registers (like DWT) :)
0 项奖励
回复
2 回复数

1,027 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed May 29 00:42:16 MST 2013

Quote: Serge
I asked the same question a little bit more than a year ago:
http://knowledgebase.nxp.com/showthread.php?t=3036

Version 3 of CMSIS was first released during the month february of 2012. Maybe it is time to reconsider the answer CodeRed?



Our position remains the same as we stated in the previous thread. Thus new part families that we have added support for over the last year or so (for example LPC800) have had their CMSIS library projects based on CMSIS 3.01. Such projects have filenames of the form CMSIS_CORE_[I]<partfamily>[/I].

Going forward, we do intend to start to use CMSIS 3.20 for new part support. But we don't intend to go back and retrofit CMSIS 3.20 into part families that support already exists for.

But remember that there is nothing to stop you pulling in the code from the latest CMSIS release from ARM into your own projects if you so desire.

Regards,
CodeRedSupport
0 项奖励
回复

1,027 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Mon May 27 06:15:01 MST 2013
I asked the same question a little bit more than a year ago:
http://knowledgebase.nxp.com/showthread.php?t=3036

Version 3 of CMSIS was first released during the month february of 2012. Maybe it is time to reconsider the answer CodeRed?
0 项奖励
回复