CMSIS-Dap debugger using LPC-Link 2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS-Dap debugger using LPC-Link 2

1,367件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Thu Apr 07 07:15:23 MST 2016
Hi,

I am evaluating a third party toolchain and want to use the LPC-Link 2 debug pod.
It works!

However it only works if I first run Lpcxpresso and debug something.  So it appears that the CMSIS-DAP profile on the LPC-Link 2 is soft, downloaded each time I run the LPCxpresso debugger.

Is there a way to configure the LPC-Link 2 to always be a CMSIS-DAP pod?

Thanks,
Tony
0 件の賞賛
返信
3 返答(返信)

1,336件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,336件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Thu Apr 07 10:26:33 MST 2016
Thanks,

I am up and running...

0 件の賞賛
返信

1,336件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Thu Apr 07 07:19:33 MST 2016
Yes. See
https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-debug-probe-firmware-programming
0 件の賞賛
返信