CMSIS-DAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS-DAP

848件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Jun 05 06:22:27 MST 2015
I see that the IDE v7.8 now loads firmware CMSIS-DAP by default.

Is the (full) source code for this available as I thought (could be wrong) that CMSIS-DAP
was open source.

Regards, Mike
0 件の賞賛
返信
1 返信

829件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jun 05 06:54:37 MST 2015
The CMSIS-DAP license is Apache 2.0.

There are lots of different CMSIS-DAP implementations - it is not 'one thing'!

The CMSIS-DAP implementation used in LPC-Link2 is not available.

However, I believe that ARM (through their mbed website) have made the source for a base implementation available in the Hardware SDK.

0 件の賞賛
返信