CMSIS-DAP could not be found.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMSIS-DAP could not be found.

6,698 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Thu Sep 24 07:44:16 MST 2015
On Tuesday, I wrote and ran a couple of simple c programs learning the system. Wednesday I down loaded the drivers recommended on the bottom of page 18 of AN11517v.1.4.pdf trying to get the GUI to run. That eliminated the warning I had seen in the Devices list of my PC, but it also seems to have stopped my ability to find CMSIS-DAP. I have downloaded the LPCXpresso package at least two more times, and still cannot debug a program. What could I be doing wrong?
0 Kudos
Reply
12 Replies

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Fri Sep 25 09:57:40 MST 2015
Thanks.
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 25 09:50:50 MST 2015
Good to hear. There's really nothing of interest to a hacker in the usbdiags.cmd output.

0 Kudos
Reply

6,581 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Fri Sep 25 09:21:54 MST 2015
I found the problem. I was plugged into the wrong MicroUSB connector on the LPC1549 Development board. I had started out plugged into J5 but the AN11517v.1.4.pdf told me to plug into J3. I switched back to J5 and now I can compile and run my initial test program. Sorry for all the time it took to remember that I had made that change trying to get the GUI to work.

Should the above postings be removed to exposing any secrets in the output from my computer tests that could endanger my computer from hackers or reveal secrets?
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 25 08:30:00 MST 2015
An unbooted LPC-Link2 probe would show up as:
VID: 1FC9 PID: 000C (LPC based USB device).

Once a CMSIS-DAP probe has been DFU'd, you would see:
VID: 1FC9 PID: 0090 (CMSIS-DAP)

The usbdiags output shows neither of these. So, your LPC1549 board just doesn't show up, either as a DFU capable device or CMSIS-DAP probe. I presume you've tried switching USB ports by this time? Do you have another board to try?

To double check your jumper settings, the following jumper connection should apply to both Rev. B, and Rev. C boards for debug of the "on-board" LPC1549.

LPC1549 Xpresso v2 Rev. B, C
JP1 Open
JP2 1-2 should be connected for "on-board" target
JP3 Open

Thanks and regards,
LPCXpresso Support


EDIT: If there's any chance the processor on the LPC-LInk2 circuit has been flashed (vs. always used as DFU), then you would need to short JP3 to force a DFU boot.
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Fri Sep 25 08:07:52 MST 2015
I am using the LPCXpresso1549 board. I have been running with LPCXpresso v7.9.2_493, which I believe uses link2 to call CMSIS-DAP for the debuging. I do not have a jumper on jp3. I did not remove that jumper, and I was able to debug on Tuesday. Should I put a jumper on jp3 and try again? Well I tried it, and CMSIS-DAP could not be found again, so I will try your other suggestions.
The first run of Usbdiags gave:

Tasks:

Image Name                     PID Services                                   
========================= ======== ============================================
System Idle Process              0 N/A                                        
System                           4 N/A                                        
smss.exe                       360 N/A                                        
csrss.exe                      484 N/A                                        
wininit.exe                    544 N/A                                        
csrss.exe                      568 N/A                                        
services.exe                   600 N/A                                        
lsass.exe                      620 KeyIso, Netlogon, SamSs                    
lsm.exe                        628 N/A                                        
winlogon.exe                   716 N/A                                        
svchost.exe                    784 DcomLaunch, PlugPlay, Power                
nvvsvc.exe                     848 NVSvc                                      
svchost.exe                    888 RpcEptMapper, RpcSs                        
svchost.exe                    976 AudioSrv, Dhcp, eventlog, lmhosts, wscsvc  
svchost.exe                    376 AudioEndpointBuilder, CscService, hidserv, 
                                   Netman, PcaSvc, SysMain, TrkWks, UxSms,    
                                   Wlansvc, wudfsvc                           
svchost.exe                    404 EventSystem, FontCache, netprofm, nsi,     
                                   W32Time, WdiServiceHost, WinHttpAutoProxySv
svchost.exe                    684 AeLookupSvc, Appinfo, BDESVC, BITS,        
                                   Browser, CertPropSvc, EapHost, IKEEXT,     
                                   iphlpsvc, LanmanServer, MMCSS, ProfSvc,    
                                   Schedule, SENS, ShellHWDetection, Themes,  
                                   Winmgmt, wuauserv                          
svchost.exe                   1128 gpsvc                                      
vpnagent.exe                  1272 vpnagent                                   
svchost.exe                   1356 CryptSvc, Dnscache, LanmanWorkstation,     
                                   NlaSvc                                     
wlanext.exe                   1460 N/A                                        
conhost.exe                   1468 N/A                                        
spoolsv.exe                   1564 Spooler                                    
svchost.exe                   1592 SCardSvr, SSDPSRV, TBS                     
svchost.exe                   1632 BFE, DPS, MpsSvc                           
armsvc.exe                    1748 AdobeARMservice                            
AESTSr64.exe                  1776 AESTFilters                                
svchost.exe                   1820 AppHostSvc                                 
atashost.exe                  1844 atashost                                   
Chaoss.exe                    1984 CHAOSS                                     
NvXDSync.exe                  1652 N/A                                        
nvvsvc.exe                    1692 N/A                                        
ehost.exe                     2256 ehost                                      
EvtEng.exe                    2276 EvtEng                                     
BLHealthMon.exe               2300 HLTHMON                                    
lkads.exe                     2460 lkClassAds                                 
magent.exe                    2504 magent                                     
nimxs.exe                     2556 mxssvr                                     
SMSvcHost.exe                 2616 NetPipeActivator, NetTcpActivator,         
                                   NetTcpPortSharing                          
nipalsm.exe                   2824 ni488enumsvc                               
niauth_daemon.exe             2844 niauth                                     
nidmsrv.exe                   2876 NIDomainService                            
NwmSvc.exe                    3012 NightWatchman50                            
nisvcloc.exe                  2324 NiSvcLoc                                   
tagsrv.exe                    2472 NITaggerService                            
o2flash.exe                   2904 O2FLASH                                    
RegSrvc.exe                   2232 RegSrvc                                    
svchost.exe                   2208 RemoteRegistry                             
ccSvcHst.exe                  3080 SepMasterService                           
WakeUpAgt.exe                 3160 WakeUpAgt                                  
svchost.exe                   3268 W3SVC, WAS                                 
ZeroConfigService.exe         3384 ZeroConfigService                          
CcmExec.exe                   3640 CcmExec                                    
lkcitdl.exe                   3672 LkCitadelServer                            
lktsrv.exe                    3744 lkTimeSync                                 
nimdnsResponder.exe           3844 nimDNSResponder                            
nipxism.exe                   3944 nipxirmu                                   
SystemWebServer.exe           3976 NISystemWebServer                          
niLxiDiscovery.exe            4016 niLXIDiscovery                             
niDiscSvc.exe                 4060 NINetworkDiscovery                         
unsecapp.exe                  4276 N/A                                        
WmiPrvSE.exe                  4428 N/A                                        
WmiPrvSE.exe                  4472 N/A                                        
NIWebServiceContainer.exe     4736 N/A                                        
ApplicationWebServer.exe      4744 NIApplicationWebServer                     
NIWebServiceContainer.exe     4888 N/A                                        
NIWebServiceContainer.exe     5072 N/A                                        
NIWebServiceContainer.exe     4160 N/A                                        
WmiPrvSE.exe                  1404 N/A                                        
Smc.exe                       1256 SmcService                                 
WUDFHost.exe                  5292 N/A                                        
svchost.exe                   5388 PolicyAgent                                
NIWebServiceContainer.exe     5632 N/A                                        
NIWebServiceContainer.exe     5672 N/A                                        
WmiPrvSE.exe                  5776 N/A                                        
SearchIndexer.exe             2604 WSearch                                    
ccSvcHst.exe                  1240 N/A                                        
taskhost.exe                  3828 N/A                                        
dwm.exe                       1228 N/A                                        
explorer.exe                  5740 N/A                                        
Apoint.exe                    3212 N/A                                        
sttray64.exe                  4860 N/A                                        
nierserver.exe                5948 N/A                                        
communicator.exe              6292 N/A                                        
vpnui.exe                     6316 N/A                                        
ApMsgFwd.exe                  6368 N/A                                        
PTIM.exe                      6376 N/A                                        
hidfind.exe                   6440 N/A                                        
ptSrv.exe                     6464 N/A                                        
ApntEx.exe                    6472 N/A                                        
conhost.exe                   6504 N/A                                        
NwmCli.exe                    6204 N/A                                        
UcMapi.exe                    7476 N/A                                        
OSPPSVC.EXE                   7676 osppsvc                                    
SMSCliUI.exe                  5796 N/A                                        
javaw.exe                     2140 N/A                                        
javaw.exe                     4580 N/A                                        
iexplore.exe                  7880 N/A                                        
FlashUtil32_14_0_0_176_Ac     7952 N/A                                        
iexplore.exe                  6340 N/A                                        
cmd.exe                       7732 N/A                                        
conhost.exe                   4872 N/A                                        
notepad.exe                   8592 N/A                                        
chrome.exe                    3044 N/A                                        
chrome.exe                    4840 N/A                                        
chrome.exe                    9004 N/A                                        
OUTLOOK.EXE                   9000 N/A                                        
audiodg.exe                   7444 N/A                                        
lpcxpresso.exe                1788 N/A                                        
taskeng.exe                   5548 N/A                                        
tasklist.exe                  7148 N/A                                        
USB Devices:
VID: 413C PID: 2110 (USB Input Device)
VID: 413C PID: 2513 (Generic USB Hub)
VID: 413C PID: 1010 (Generic USB Hub)
VID: 413C PID: 2513 (Generic USB Hub)
VID: 413C PID: 2110 (HID-compliant device)
VID: 8087 PID: 0024 (Generic USB Hub)
VID: 413C PID: 2110 (HID-compliant mouse)
VID: 8087 PID: 0024 (Generic USB Hub)
VID: 0461 PID: 4D51 (HID-compliant mouse)
VID: 413C PID: 2110 (USB Composite Device)
VID: 0A5C PID: 5800 (USB Composite Device)
VID: 0A5C PID: 5800 (Dell ControlVault w/o Fingerprint Sensor)
VID: 413C PID: 2110 (HID-compliant device)
VID: 0A5C PID: 5800 (Broadcom Usbccid Smartcard Reader (WUDF))
VID: 0461 PID: 4D51 (USB Input Device)
VID: 413C PID: 2110 (USB Input Device)
VID: 413C PID: 2110 (HID Keyboard Device)
VID: 413C PID: 2110 (HID-compliant consumer control device)
DFU Devices:
HID Devices:
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant device
Device ID: HID\VID_413C&PID_2110&MI_01&COL04\A&5F1A1FC&0&0003
Manufacturer: (Standard system devices)
Name: HID-compliant device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL04\A&5F1A1FC&0&0003
Service:
Class GUID: {4d36e96f-e325-11ce-bfc1-08002be10318}
Description: HID-compliant mouse
Device ID: HID\VID_413C&PID_2110&MI_01&COL01\A&5F1A1FC&0&0000
Manufacturer: Microsoft
Name: HID-compliant mouse
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL01\A&5F1A1FC&0&0000
Service: mouhid
Class GUID: {4d36e96f-e325-11ce-bfc1-08002be10318}
Description: HID-compliant mouse
Device ID: HID\VID_0461&PID_4D51\8&34A5812&0&0000
Manufacturer: Microsoft
Name: HID-compliant mouse
PNP Device ID: HID\VID_0461&PID_4D51\8&34A5812&0&0000
Service: mouhid
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant device
Device ID: HID\VID_413C&PID_2110&MI_01&COL02\A&5F1A1FC&0&0001
Manufacturer: (Standard system devices)
Name: HID-compliant device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL02\A&5F1A1FC&0&0001
Service:
Class GUID: {4d36e96b-e325-11ce-bfc1-08002be10318}
Description: HID Keyboard Device
Device ID: HID\VID_413C&PID_2110&MI_00\A&1921BE3A&0&0000
Manufacturer: (Standard keyboards)
Name: HID Keyboard Device
PNP Device ID: HID\VID_413C&PID_2110&MI_00\A&1921BE3A&0&0000
Service: kbdhid
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant consumer control device
Device ID: HID\VID_413C&PID_2110&MI_01&COL03\A&5F1A1FC&0&0002
Manufacturer: Microsoft
Name: HID-compliant consumer control device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL03\A&5F1A1FC&0&0002
Service:


Then I ran bin/boot_links2, and ran usbdiags again giving:

Tasks:

Image Name                     PID Services                                   
========================= ======== ============================================
System Idle Process              0 N/A                                        
System                           4 N/A                                        
smss.exe                       360 N/A                                        
csrss.exe                      484 N/A                                        
wininit.exe                    544 N/A                                        
csrss.exe                      568 N/A                                        
services.exe                   600 N/A                                        
lsass.exe                      620 KeyIso, Netlogon, SamSs                    
lsm.exe                        628 N/A                                        
winlogon.exe                   716 N/A                                        
svchost.exe                    784 DcomLaunch, PlugPlay, Power                
nvvsvc.exe                     848 NVSvc                                      
svchost.exe                    888 RpcEptMapper, RpcSs                        
svchost.exe                    976 AudioSrv, Dhcp, eventlog, lmhosts, wscsvc  
svchost.exe                    376 AudioEndpointBuilder, CscService, hidserv, 
                                   Netman, PcaSvc, SysMain, TrkWks, UxSms,    
                                   Wlansvc, wudfsvc                           
svchost.exe                    404 EventSystem, FontCache, netprofm, nsi,     
                                   W32Time, WdiServiceHost                    
svchost.exe                    684 AeLookupSvc, Appinfo, BDESVC, BITS,        
                                   Browser, CertPropSvc, EapHost, IKEEXT,     
                                   iphlpsvc, LanmanServer, MMCSS, ProfSvc,    
                                   Schedule, SENS, ShellHWDetection, Themes,  
                                   Winmgmt, wuauserv                          
svchost.exe                   1128 gpsvc                                      
vpnagent.exe                  1272 vpnagent                                   
svchost.exe                   1356 CryptSvc, Dnscache, LanmanWorkstation,     
                                   NlaSvc                                     
wlanext.exe                   1460 N/A                                        
conhost.exe                   1468 N/A                                        
spoolsv.exe                   1564 Spooler                                    
svchost.exe                   1592 SCardSvr, SSDPSRV, TBS                     
svchost.exe                   1632 BFE, DPS, MpsSvc                           
armsvc.exe                    1748 AdobeARMservice                            
AESTSr64.exe                  1776 AESTFilters                                
svchost.exe                   1820 AppHostSvc                                 
atashost.exe                  1844 atashost                                   
Chaoss.exe                    1984 CHAOSS                                     
NvXDSync.exe                  1652 N/A                                        
nvvsvc.exe                    1692 N/A                                        
ehost.exe                     2256 ehost                                      
EvtEng.exe                    2276 EvtEng                                     
BLHealthMon.exe               2300 HLTHMON                                    
lkads.exe                     2460 lkClassAds                                 
magent.exe                    2504 magent                                     
nimxs.exe                     2556 mxssvr                                     
SMSvcHost.exe                 2616 NetPipeActivator, NetTcpActivator,         
                                   NetTcpPortSharing                          
nipalsm.exe                   2824 ni488enumsvc                               
niauth_daemon.exe             2844 niauth                                     
nidmsrv.exe                   2876 NIDomainService                            
NwmSvc.exe                    3012 NightWatchman50                            
nisvcloc.exe                  2324 NiSvcLoc                                   
tagsrv.exe                    2472 NITaggerService                            
o2flash.exe                   2904 O2FLASH                                    
RegSrvc.exe                   2232 RegSrvc                                    
svchost.exe                   2208 RemoteRegistry                             
ccSvcHst.exe                  3080 SepMasterService                           
WakeUpAgt.exe                 3160 WakeUpAgt                                  
svchost.exe                   3268 W3SVC, WAS                                 
ZeroConfigService.exe         3384 ZeroConfigService                          
CcmExec.exe                   3640 CcmExec                                    
lkcitdl.exe                   3672 LkCitadelServer                            
lktsrv.exe                    3744 lkTimeSync                                 
nimdnsResponder.exe           3844 nimDNSResponder                            
nipxism.exe                   3944 nipxirmu                                   
SystemWebServer.exe           3976 NISystemWebServer                          
niLxiDiscovery.exe            4016 niLXIDiscovery                             
niDiscSvc.exe                 4060 NINetworkDiscovery                         
unsecapp.exe                  4276 N/A                                        
WmiPrvSE.exe                  4428 N/A                                        
WmiPrvSE.exe                  4472 N/A                                        
NIWebServiceContainer.exe     4736 N/A                                        
ApplicationWebServer.exe      4744 NIApplicationWebServer                     
NIWebServiceContainer.exe     4888 N/A                                        
NIWebServiceContainer.exe     5072 N/A                                        
NIWebServiceContainer.exe     4160 N/A                                        
WmiPrvSE.exe                  1404 N/A                                        
Smc.exe                       1256 SmcService                                 
WUDFHost.exe                  5292 N/A                                        
svchost.exe                   5388 PolicyAgent                                
NIWebServiceContainer.exe     5632 N/A                                        
NIWebServiceContainer.exe     5672 N/A                                        
WmiPrvSE.exe                  5776 N/A                                        
SearchIndexer.exe             2604 WSearch                                    
ccSvcHst.exe                  1240 N/A                                        
taskhost.exe                  3828 N/A                                        
dwm.exe                       1228 N/A                                        
explorer.exe                  5740 N/A                                        
Apoint.exe                    3212 N/A                                        
sttray64.exe                  4860 N/A                                        
nierserver.exe                5948 N/A                                        
communicator.exe              6292 N/A                                        
vpnui.exe                     6316 N/A                                        
ApMsgFwd.exe                  6368 N/A                                        
PTIM.exe                      6376 N/A                                        
hidfind.exe                   6440 N/A                                        
ptSrv.exe                     6464 N/A                                        
ApntEx.exe                    6472 N/A                                        
conhost.exe                   6504 N/A                                        
NwmCli.exe                    6204 N/A                                        
UcMapi.exe                    7476 N/A                                        
OSPPSVC.EXE                   7676 osppsvc                                    
SMSCliUI.exe                  5796 N/A                                        
javaw.exe                     2140 N/A                                        
javaw.exe                     4580 N/A                                        
iexplore.exe                  7880 N/A                                        
FlashUtil32_14_0_0_176_Ac     7952 N/A                                        
iexplore.exe                  6340 N/A                                        
cmd.exe                       7732 N/A                                        
conhost.exe                   4872 N/A                                        
notepad.exe                   8592 N/A                                        
chrome.exe                    3044 N/A                                        
chrome.exe                    4840 N/A                                        
chrome.exe                    9004 N/A                                        
OUTLOOK.EXE                   9000 N/A                                        
audiodg.exe                   7444 N/A                                        
lpcxpresso.exe                1788 N/A                                        
tasklist.exe                  8600 N/A                                        
USB Devices:
VID: 413C PID: 2110 (USB Input Device)
VID: 0403 PID: 6001 (USB Serial Converter)
VID: 413C PID: 2513 (Generic USB Hub)
VID: 413C PID: 1010 (Generic USB Hub)
VID: 413C PID: 2513 (Generic USB Hub)
VID: 413C PID: 2110 (HID-compliant device)
VID: 8087 PID: 0024 (Generic USB Hub)
VID: 413C PID: 2110 (HID-compliant mouse)
VID: 8087 PID: 0024 (Generic USB Hub)
VID: 0461 PID: 4D51 (HID-compliant mouse)
VID: 413C PID: 2110 (USB Composite Device)
VID: 0A5C PID: 5800 (USB Composite Device)
VID: 0A5C PID: 5800 (Dell ControlVault w/o Fingerprint Sensor)
VID: 413C PID: 2110 (HID-compliant device)
VID: 0403 PID: 6001 (USB Serial Port)
VID: 0A5C PID: 5800 (Broadcom Usbccid Smartcard Reader (WUDF))
VID: 0461 PID: 4D51 (USB Input Device)
VID: 413C PID: 2110 (USB Input Device)
VID: 413C PID: 2110 (HID Keyboard Device)
VID: 413C PID: 2110 (HID-compliant consumer control device)
DFU Devices:
HID Devices:
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant device
Device ID: HID\VID_413C&PID_2110&MI_01&COL04\A&5F1A1FC&0&0003
Manufacturer: (Standard system devices)
Name: HID-compliant device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL04\A&5F1A1FC&0&0003
Service:
Class GUID: {4d36e96f-e325-11ce-bfc1-08002be10318}
Description: HID-compliant mouse
Device ID: HID\VID_413C&PID_2110&MI_01&COL01\A&5F1A1FC&0&0000
Manufacturer: Microsoft
Name: HID-compliant mouse
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL01\A&5F1A1FC&0&0000
Service: mouhid
Class GUID: {4d36e96f-e325-11ce-bfc1-08002be10318}
Description: HID-compliant mouse
Device ID: HID\VID_0461&PID_4D51\8&34A5812&0&0000
Manufacturer: Microsoft
Name: HID-compliant mouse
PNP Device ID: HID\VID_0461&PID_4D51\8&34A5812&0&0000
Service: mouhid
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant device
Device ID: HID\VID_413C&PID_2110&MI_01&COL02\A&5F1A1FC&0&0001
Manufacturer: (Standard system devices)
Name: HID-compliant device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL02\A&5F1A1FC&0&0001
Service:
Class GUID: {4d36e96b-e325-11ce-bfc1-08002be10318}
Description: HID Keyboard Device
Device ID: HID\VID_413C&PID_2110&MI_00\A&1921BE3A&0&0000
Manufacturer: (Standard keyboards)
Name: HID Keyboard Device
PNP Device ID: HID\VID_413C&PID_2110&MI_00\A&1921BE3A&0&0000
Service: kbdhid
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant consumer control device
Device ID: HID\VID_413C&PID_2110&MI_01&COL03\A&5F1A1FC&0&0002
Manufacturer: Microsoft
Name: HID-compliant consumer control device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL03\A&5F1A1FC&0&0002
Service:


The only thing I saw different was the line:
VID: 0403 PID: 6001 (USB Serial Converter)
was added in the second output.
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 25 06:50:12 MST 2015
Please take a step back and first of all can you confirm what your actual target and debug probe are?

Are you using an LPCXpresso1549 board (and its built in LPC-Link2 debug probe), or are you using a different debug probe (for example a standalone LPC-Link2) and a different board?

If you are using an LPCXpresso1549 board, then please ensure that you have jumper fitted on JP3.

If you are using a standalone LPC-Link2 probe, then please ensure that you [u]do not[/u] have a jumper fitted on JP1.

Now unplug every USB device that you can from your PC, including your debug probe/target board.

Now open a DOS command prompt and run the command:

{install_dir}\lpcxpresso\bin\Scripts\usbdiags > diag1.txt


(where {install_dir} is your LPCXpresso 7.9.2 installation directory)

Now connect your debug probe/board and run the boot_link2 script

Now in the DOS command prompt run the command:

{install_dir}\lpcxpresso\bin\Scripts\usbdiags > diag2.txt


And post the diag1.txt  and diag2.txt files that have been  generated for us to look at.

Please also go through the troubleshooting in this FAQ and let us know if anything here helps:

https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link2

Regards,
LPCXpresso Support
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Fri Sep 25 05:13:01 MST 2015
Before attempting to run boot_link2.com
USB the port (COM7) driver is:
Driver Provider:FRDI
Driver Date:7/10/2015
Driver Version:2.12.6.0
Digital Signer:Microsoft Windows Hardware Compatibility Publisher

After issuing the command: boot_link2
and receiving "Nothing to boot"

The driver for USB port (Com 7) is:
Driver Provider:FRDI
Driver Date:7/10/2015
Driver Version:2.12.6.0
Digital Signer:Microsoft Windows Hardware Compatibility Publisher

So I did not report that, because it did not change, so I thought the test failed.

Because I did not get a response I did some investigation on my own. I made a copy of boot_link2.cmd (so I did not mess it up) as Link2up.cmd and edited out the @echo off line. I ran that and this is the output which I thought might tell you something:

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>setlocal enabledelayedexpansion

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set BootHome=C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin\

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set DeviceName=LPC-Link2

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set BootImageWildBridge=LPC432x_Redlink_V*.hdr 

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set BootImageWildNonBridge=LPC432x_Redlink_NB_V*.hdr 

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set BootImageWildCmsisDap=LPC432x_CMSIS_DAP_V*.hdr 

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set BootImageWildCmsisDapNonBridge=LPC432x_CMSIS_DAP_NB_V*.hdr 

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set DfuLog=C:\Users\tpotter1\AppData\Local\Temp\dfu-util.log

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>if /I "" == "help" goto :Usage

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>set BootImage=

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>if "" == "" set BootImage=CMSIS

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>call :getDfuVidPid

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>for /F "skip=6 tokens=3" %a in ('C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin\dfu-util -l') do (set DfuVidPid=%a )

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>goto :eof

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>if "" == "" goto :NoDfus

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>echo Nothing to boot!
Nothing to boot

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>goto :end

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>endlocal

C:\nxp\LPCXpresso_7.9.2_493\lpcxpresso\bin>goto :eof


Now for the suggestion that you sent after I went home for the night.
I ran the usdiags.cmd and here is the ouput you wanted:
Tasks:

Image Name                     PID Services                                   
========================= ======== ============================================
System Idle Process              0 N/A                                        
System                           4 N/A                                        
smss.exe                       360 N/A                                        
csrss.exe                      484 N/A                                        
wininit.exe                    544 N/A                                        
csrss.exe                      568 N/A                                        
services.exe                   600 N/A                                        
lsass.exe                      620 KeyIso, Netlogon, SamSs                    
lsm.exe                        628 N/A                                        
winlogon.exe                   716 N/A                                        
svchost.exe                    784 DcomLaunch, PlugPlay, Power                
nvvsvc.exe                     848 NVSvc                                      
svchost.exe                    888 RpcEptMapper, RpcSs                        
svchost.exe                    976 AudioSrv, Dhcp, eventlog, lmhosts, wscsvc  
svchost.exe                    376 AudioEndpointBuilder, CscService, hidserv, 
                                   Netman, PcaSvc, SysMain, TrkWks, UxSms,    
                                   Wlansvc, wudfsvc                           
svchost.exe                    404 EventSystem, FontCache, netprofm, nsi,     
                                   W32Time, WdiServiceHost, WinHttpAutoProxySv
svchost.exe                    684 AeLookupSvc, Appinfo, BDESVC, BITS,        
                                   Browser, CertPropSvc, EapHost, IKEEXT,     
                                   iphlpsvc, LanmanServer, ProfSvc, Schedule, 
                                   SENS, ShellHWDetection, Themes, Winmgmt,   
                                   wuauserv                                   
svchost.exe                   1128 gpsvc                                      
vpnagent.exe                  1272 vpnagent                                   
svchost.exe                   1356 CryptSvc, Dnscache, LanmanWorkstation,     
                                   NlaSvc                                     
wlanext.exe                   1460 N/A                                        
conhost.exe                   1468 N/A                                        
spoolsv.exe                   1564 Spooler                                    
svchost.exe                   1592 SCardSvr, SSDPSRV, TBS                     
svchost.exe                   1632 BFE, DPS, MpsSvc                           
armsvc.exe                    1748 AdobeARMservice                            
AESTSr64.exe                  1776 AESTFilters                                
svchost.exe                   1820 AppHostSvc                                 
atashost.exe                  1844 atashost                                   
Chaoss.exe                    1984 CHAOSS                                     
NvXDSync.exe                  1652 N/A                                        
nvvsvc.exe                    1692 N/A                                        
ehost.exe                     2256 ehost                                      
EvtEng.exe                    2276 EvtEng                                     
BLHealthMon.exe               2300 HLTHMON                                    
lkads.exe                     2460 lkClassAds                                 
magent.exe                    2504 magent                                     
nimxs.exe                     2556 mxssvr                                     
SMSvcHost.exe                 2616 NetPipeActivator, NetTcpActivator,         
                                   NetTcpPortSharing                          
nipalsm.exe                   2824 ni488enumsvc                               
niauth_daemon.exe             2844 niauth                                     
nidmsrv.exe                   2876 NIDomainService                            
NwmSvc.exe                    3012 NightWatchman50                            
nisvcloc.exe                  2324 NiSvcLoc                                   
tagsrv.exe                    2472 NITaggerService                            
o2flash.exe                   2904 O2FLASH                                    
RegSrvc.exe                   2232 RegSrvc                                    
svchost.exe                   2208 RemoteRegistry                             
ccSvcHst.exe                  3080 SepMasterService                           
WakeUpAgt.exe                 3160 WakeUpAgt                                  
svchost.exe                   3268 W3SVC, WAS                                 
ZeroConfigService.exe         3384 ZeroConfigService                          
CcmExec.exe                   3640 CcmExec                                    
lkcitdl.exe                   3672 LkCitadelServer                            
lktsrv.exe                    3744 lkTimeSync                                 
nimdnsResponder.exe           3844 nimDNSResponder                            
nipxism.exe                   3944 nipxirmu                                   
SystemWebServer.exe           3976 NISystemWebServer                          
niLxiDiscovery.exe            4016 niLXIDiscovery                             
niDiscSvc.exe                 4060 NINetworkDiscovery                         
unsecapp.exe                  4276 N/A                                        
WmiPrvSE.exe                  4428 N/A                                        
WmiPrvSE.exe                  4472 N/A                                        
NIWebServiceContainer.exe     4736 N/A                                        
ApplicationWebServer.exe      4744 NIApplicationWebServer                     
NIWebServiceContainer.exe     4888 N/A                                        
NIWebServiceContainer.exe     5072 N/A                                        
NIWebServiceContainer.exe     4160 N/A                                        
WmiPrvSE.exe                  1404 N/A                                        
Smc.exe                       1256 SmcService                                 
WUDFHost.exe                  5292 N/A                                        
svchost.exe                   5388 PolicyAgent                                
NIWebServiceContainer.exe     5632 N/A                                        
NIWebServiceContainer.exe     5672 N/A                                        
WmiPrvSE.exe                  5776 N/A                                        
SearchIndexer.exe             2604 WSearch                                    
ccSvcHst.exe                  1240 N/A                                        
taskhost.exe                  3828 N/A                                        
dwm.exe                       1228 N/A                                        
explorer.exe                  5740 N/A                                        
Apoint.exe                    3212 N/A                                        
sttray64.exe                  4860 N/A                                        
nierserver.exe                5948 N/A                                        
communicator.exe              6292 N/A                                        
vpnui.exe                     6316 N/A                                        
ApMsgFwd.exe                  6368 N/A                                        
PTIM.exe                      6376 N/A                                        
hidfind.exe                   6440 N/A                                        
ptSrv.exe                     6464 N/A                                        
ApntEx.exe                    6472 N/A                                        
conhost.exe                   6504 N/A                                        
NwmCli.exe                    6204 N/A                                        
UcMapi.exe                    7476 N/A                                        
OSPPSVC.EXE                   7676 osppsvc                                    
SMSCliUI.exe                  5796 N/A                                        
javaw.exe                     2140 N/A                                        
javaw.exe                     4580 N/A                                        
iexplore.exe                  7880 N/A                                        
iexplore.exe                  2612 N/A                                        
FlashUtil32_14_0_0_176_Ac     7952 N/A                                        
iexplore.exe                  6340 N/A                                        
cmd.exe                       7732 N/A                                        
conhost.exe                   4872 N/A                                        
notepad.exe                   7728 N/A                                        
tasklist.exe                  1368 N/A                                        
USB Devices:
VID: 413C PID: 2110 (USB Input Device)
VID: 0403 PID: 6001 (USB Serial Converter)
VID: 413C PID: 2513 (Generic USB Hub)
VID: 413C PID: 1010 (Generic USB Hub)
VID: 413C PID: 2513 (Generic USB Hub)
VID: 413C PID: 2110 (HID-compliant device)
VID: 8087 PID: 0024 (Generic USB Hub)
VID: 413C PID: 2110 (HID-compliant mouse)
VID: 8087 PID: 0024 (Generic USB Hub)
VID: 0461 PID: 4D51 (HID-compliant mouse)
VID: 413C PID: 2110 (USB Composite Device)
VID: 0A5C PID: 5800 (USB Composite Device)
VID: 0A5C PID: 5800 (Dell ControlVault w/o Fingerprint Sensor)
VID: 413C PID: 2110 (HID-compliant device)
VID: 0403 PID: 6001 (USB Serial Port)
VID: 0A5C PID: 5800 (Broadcom Usbccid Smartcard Reader (WUDF))
VID: 0461 PID: 4D51 (USB Input Device)
VID: 413C PID: 2110 (USB Input Device)
VID: 413C PID: 2110 (HID Keyboard Device)
VID: 413C PID: 2110 (HID-compliant consumer control device)
DFU Devices:
HID Devices:
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant device
Device ID: HID\VID_413C&PID_2110&MI_01&COL04\A&5F1A1FC&0&0003
Manufacturer: (Standard system devices)
Name: HID-compliant device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL04\A&5F1A1FC&0&0003
Service:
Class GUID: {4d36e96f-e325-11ce-bfc1-08002be10318}
Description: HID-compliant mouse
Device ID: HID\VID_413C&PID_2110&MI_01&COL01\A&5F1A1FC&0&0000
Manufacturer: Microsoft
Name: HID-compliant mouse
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL01\A&5F1A1FC&0&0000
Service: mouhid
Class GUID: {4d36e96f-e325-11ce-bfc1-08002be10318}
Description: HID-compliant mouse
Device ID: HID\VID_0461&PID_4D51\8&34A5812&0&0000
Manufacturer: Microsoft
Name: HID-compliant mouse
PNP Device ID: HID\VID_0461&PID_4D51\8&34A5812&0&0000
Service: mouhid
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant device
Device ID: HID\VID_413C&PID_2110&MI_01&COL02\A&5F1A1FC&0&0001
Manufacturer: (Standard system devices)
Name: HID-compliant device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL02\A&5F1A1FC&0&0001
Service:
Class GUID: {4d36e96b-e325-11ce-bfc1-08002be10318}
Description: HID Keyboard Device
Device ID: HID\VID_413C&PID_2110&MI_00\A&1921BE3A&0&0000
Manufacturer: (Standard keyboards)
Name: HID Keyboard Device
PNP Device ID: HID\VID_413C&PID_2110&MI_00\A&1921BE3A&0&0000
Service: kbdhid
Class GUID: {745a17a0-74d3-11d0-b6fe-00a0c90f57da}
Description: HID-compliant consumer control device
Device ID: HID\VID_413C&PID_2110&MI_01&COL03\A&5F1A1FC&0&0002
Manufacturer: Microsoft
Name: HID-compliant consumer control device
PNP Device ID: HID\VID_413C&PID_2110&MI_01&COL03\A&5F1A1FC&0&0002
Service:


I will be anxious to see what that tells you. Thanks for working with me on this, Tim0855.
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Sep 24 14:34:00 MST 2015
You didn't answer whether you found an obsolete UCOM driver installed? If the CMSIS-DAP probe is already booted, you'll get the same message. Reproduce the fail message after using the boot_link2.cmd script, then open an MS-DOS shell and run the usbdiags.cmd script found in the '<install>\lpcxpresso\bin\Scripts' folder. Paste the console output in your next response.

Thanks and regards,
LPCXpresso Support
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Thu Sep 24 10:04:08 MST 2015
When I entered boot_link2, the system replied "Nothing to boot" but I can see boot_link2.cmd is in the directory, and typing it shows there are commands in the file. I am confused.
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Sep 24 08:45:52 MST 2015
If you are using an LPC-Link2 (either standalone or the one built into an LPCXpresso1549 or similar board), then the most likely issue is this one:

https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-failing-enumerate-cmsis-dap-firmware

Regards,
LPCXpresso Support
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tim0855 on Thu Sep 24 08:01:44 MST 2015
I am running the LPC1549 chip from a Dell Laptop running Windows 7 with a Ford Load (which could be an issue).
0 Kudos
Reply

6,580 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Sep 24 07:47:58 MST 2015
Any hint about your hardware?
0 Kudos
Reply