CLOCK speed problem during debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLOCK speed problem during debug

1,034件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dr Whom on Thu Mar 18 06:23:41 MST 2010
Hello

I have a problem when running single wire debug through a J link and an LPC 1313

During debug mode with IAR, my Clock out is exactly 10 Mhz and outside the debug it is the expected 12 Mhz from Internal RC.

Anybody run into this already?
0 件の賞賛
返信
2 返答(返信)

1,001件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dr Whom on Tue Mar 23 05:53:29 MST 2010

Quote: Dr Whom
Hello

I have a problem when running single wire debug through a J link and an LPC 1313

During debug mode with IAR, my Clock out is exactly 10 Mhz and outside the debug it is the expected 12 Mhz from Internal RC.

Anybody run into this already?



FYI

My problem was that my J-link needed to be set for 'Halt after bootloader'

If the bootloader does not run, it will not load the trim values for the internal RC to give you 12 Mhz
0 件の賞賛
返信

1,001件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Fri Mar 19 11:49:26 MST 2010
Hello,

I have not had that problem.
LPC1343 and CodeRed IDE.
0 件の賞賛
返信