CAN protocol code for LPC2129

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN protocol code for LPC2129

1,655 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Sun May 13 22:40:27 MST 2012
Hi....!!!
Please share the C code or Sample Code for CAN protocol for LPC2129 if anybody is having it.It is OK if it works on Keil platform also.


Thanks & Regards.....:)
0 Kudos
Reply
2 Replies

1,407 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Mon May 14 22:15:37 MST 2012

Quote: Polux rsv
A simple Google search with "can LPC2129" would give you tons of links :rolleyes:
And there is a good Yahoo group called....LPC2000 :D with lots of examples. LPC2129_Canall is one of them
And I remember the CAN interface on LPC2129 has a bug in the transmitter.

Angelo


@Polux rsv...Hi..!!!

Thanks a lot for your kind reply.

Thanks & Regards....!!!:)
0 Kudos
Reply

1,407 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Mon May 14 08:13:24 MST 2012
A simple Google search with "can LPC2129" would give you tons of links :rolleyes:
And there is a good Yahoo group called....LPC2000 :D with lots of examples. LPC2129_Canall is one of them
And I remember the CAN interface on LPC2129 has a bug in the transmitter.

Angelo
0 Kudos
Reply