Build error with LPC expresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build error with LPC expresso IDE

1,956件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vineetrvce on Mon Mar 19 07:28:33 MST 2012
Hello,
  I am trying to build the imported code from lpc expresso, but it fails after giving this error:

[COLOR=Red]**** Build of configuration Debug for project i2c ****

make all
      0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0x0, BaseAddress 0x71110000, RegionSize 0x100000, State 0x10000
D:\nxp\LPCXpresso_4.0.6_152\lpcxpresso\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0[/COLOR]

Has anyone faced this issue. Please suggest.

Thanks,
Vineet.
0 件の賞賛
返信
5 返答(返信)

1,846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Jan 27 00:22:55 MST 2013

Quote: manishd
The link is broken.



:confused:

http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull

is working here without problem :)
0 件の賞賛
返信

1,846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by manishd on Sat Jan 26 22:45:00 MST 2013
The link is broken.
0 件の賞賛
返信

1,846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vineetrvce on Wed Mar 28 02:34:13 MST 2012
Sorry if I have reposted the problem. Following code red instrutions I am able to solve the issue by replacing the .dll file.
0 件の賞賛
返信

1,846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tom84 on Tue Mar 20 01:49:23 MST 2012
Perhaps this may help you

http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull
0 件の賞賛
返信

1,846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Mar 19 07:34:03 MST 2012
1. Try search the forum, or
2. Try searching the FAQ...

This question has been asked and answered several times...
0 件の賞賛
返信