Build does not compile all .C Files in the Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build does not compile all .C Files in the Project

1,002 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by siro on Mon Dec 01 08:02:05 MST 2014
Build does not compile all .C Files in my Project
Hello,
i have a working C-Project (compiled and testes with IAR) with some .C Files without Libraries.

i put All  these Files in the project workspace .SRC directory
If i Build my project, i get Problems.
i have tested anything and can locate that the build process has not compiled somes files.
i can found, that the IDE generates a file SUBDIR.MK and here i found that some files of my project are not shown.
If have checked in the IDE that these Files are not excludes from build.

i get erros undefined reference xxxxx
and i see this is okay, because the compiler has not compiled some files and so there were no Objectfiles generated.

I can also see in the comsole window, that some files are not compiled.

For testing i have dowmload and installed an older version of the IDE 6.xx
there is the same problem with the newest version IDE 7.5

i dont know where is the problem.
can everybody help me, to resolve my problem

Bernd

0 Kudos
Reply
2 Replies

932 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by siro on Mon Dec 01 08:54:08 MST 2014
Oh yes,
you are right.

the IAR-IDE  ignores the .c  .C

i searched some days for the reason.....

very thanks.
Bernd
0 Kudos
Reply

932 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Dec 01 08:29:30 MST 2014
C files must have an extension of ".c" and not ".C". i.e use lower-case file extensions.
0 Kudos
Reply