Build Last Project Hotkey

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Last Project Hotkey

1,060件の閲覧回数
simonwyss
Contributor III

Is there a possibility to setup a hotkey for the build "my project" [Debug] button?
I do not find this command in Window /Preferences /General /Keys

However there is a command "Build Project". This works only if I select first the project folder.

pastedImage_3.png

For debug I used the the command "Debug Last Launched".

pastedImage_2.png

But I do not want to start debuging if I only need to build the project.

Is there a solution to add a hotkey to the Build "my project" button?

pastedImage_4.png

0 件の賞賛
返信
0 返答(返信)