Build Last Project Hotkey

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build Last Project Hotkey

1,066 Views
simonwyss
Contributor III

Is there a possibility to setup a hotkey for the build "my project" [Debug] button?
I do not find this command in Window /Preferences /General /Keys

However there is a command "Build Project". This works only if I select first the project folder.

pastedImage_3.png

For debug I used the the command "Debug Last Launched".

pastedImage_2.png

But I do not want to start debuging if I only need to build the project.

Is there a solution to add a hotkey to the Build "my project" button?

pastedImage_4.png

0 Kudos
Reply
0 Replies