Break display format value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Break display format value

855 次查看
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by blasiis on Wed Jul 21 05:16:27 MST 2010
Where can I find to configure the value display format when I am breaked.
I need the hex format !
I cannot find this setting !

Thanks

http://file///C:/Documents%20and%20Settings/Stefano.PORTORICO/Desktop/format.bmp

0 项奖励
回复
4 回复数

798 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Jul 21 23:21:28 MST 2010

Quote: CodeRedSupport
Sorry, eclipse seems to have no way to change the format of variables as displayed in tooltips - only the display in the register, variables, etc views.



OK :mad:
0 项奖励
回复

798 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jul 21 14:01:13 MST 2010
Sorry, eclipse seems to have no way to change the format of variables as displayed in tooltips - only the display in the register, variables, etc views.
0 项奖励
回复

798 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Wed Jul 21 05:32:53 MST 2010
All this value is already set ti hexadecimal but the display value i decimal !!
0 项奖励
回复

798 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jul 21 05:20:55 MST 2010
See the knowledgebase entry "IDE Config : Default display formats" at:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/53
[login required]

Regards,
CodeRedSupport
0 项奖励
回复