Board Schematic Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board Schematic Problem

1,682 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by camarena on Wed Sep 15 11:40:59 MST 2010
[IMG]file:///C:/Users/ACAMAR%7E1.AND/AppData/Local/Temp/moz-screenshot-3.png[/IMG]I cannot communicate with the board. I am using an lpc1769 and  lpcxpresso programmer. Do I need to plug in trst or rstoutn to anything?
0 Kudos
Reply
2 Replies

1,660 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pig_man on Mon Sep 20 09:02:35 MST 2010
Did you try to pull up the TRST line with a 10k to Vcc?

Can you see the device ID from the message box?
0 Kudos
Reply

1,660 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Sep 15 12:09:25 MST 2010
LPCXpresso (LPC-Link) is using SWD:

SWDCLK
SWDIO
Ground

That's all you need :)
0 Kudos
Reply