Beginner question for timer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Beginner question for timer

695 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MCU on Tue Apr 02 21:14:46 MST 2013
Hi,
I'm beginner for LPC,
I using LPCxpresso LPC1200 Rev B
I want to do a simple program, enable the 32bit timer counter and output the high low in port
So, I need to know how to set up the CT32B0,
I already enable the counter, but I don;t know the system clock speed.
If I not change the CMISS, did the system clock 24MHZ?
So the timer counter will update every 1/24MHZ?
1) Any sample code for it?
If I use the Blinky sample code as a base.
2) did I need to disable all the interrupt?
3) did I need to reset the watch dog?
0 Kudos
Reply
1 Reply

683 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Apr 04 00:47:41 MST 2013
There are code examples provided in the LPCXpresso Examples subdirectory for various parts (though not currently LPC12). However the code for LPC11, for example, should be easily adaptable.

You could also check out previous posts on the forum using the sticky post at the top of the thread list. For example, this thread may well be useful...

http://knowledgebase.nxp.com/showthread.php?t=3867

Also there is some information on the LPC12 watchdog and "support" for it in LPCXpresso at:

http://support.code-red-tech.com/CodeRedWiki/LPC12Watchdog

Regards,
CodeRedSupport
0 Kudos
Reply