Basic project using CMSIS...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basic project using CMSIS...

1,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Oct 29 07:49:35 MST 2014
Hi,

I understand there is something called LPCOpen that is intended to replace CMSIS. How do I avoid using that? I just want to use the standard portable CMSIS libraries...

Thank you in advance.

-Nate
0 Kudos
Reply
2 Replies

1,019 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Fri Oct 31 09:28:02 MST 2014
OK, thanks! I'm using what was in the lpcopen_2_01_keil_iar_nxp_lpcxpresso_812.zip...
0 Kudos
Reply

1,019 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed Oct 29 08:50:28 MST 2014
Hello
It really depends which device type you are interested in using.  Some devices, like the LPC11xx family, do have CMSIS libraries.  You can find an example at http://www.lpcware.com/node/11538/58.
For the newer devices, we suggest using LPCOpen as we no longer support the old style CMSIS libraries.

Regards
Paul
0 Kudos
Reply