Auto update .DIS when building Assembler program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Auto update .DIS when building Assembler program

485件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by acelink1 on Thu Feb 27 23:15:26 MST 2014
Hi Guys, I noticed that when I build my Assembler project in Xpresso the .dis window is not being updated with
the new assembler code.

I have to manually right click on the assem.o then choose Binary Utilities then Disassemble.
Only then it updates the Disassembly window.

I just want to know is there a way to automatically update the disassembly window when I build my Assembler program
or doesn't Xpresso have this feature?

I'm new to LPC 4357 and Xpresso and so far I find it to be absolutely fantastic :) 

Thanks Guys

Pete :)
0 件の賞賛
返信
0 返答(返信)