Auto update .DIS when building Assembler program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Auto update .DIS when building Assembler program

484 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by acelink1 on Thu Feb 27 23:15:26 MST 2014
Hi Guys, I noticed that when I build my Assembler project in Xpresso the .dis window is not being updated with
the new assembler code.

I have to manually right click on the assem.o then choose Binary Utilities then Disassemble.
Only then it updates the Disassembly window.

I just want to know is there a way to automatically update the disassembly window when I build my Assembler program
or doesn't Xpresso have this feature?

I'm new to LPC 4357 and Xpresso and so far I find it to be absolutely fantastic :) 

Thanks Guys

Pete :)
0 Kudos
Reply
0 Replies