Always debug error occurs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Always debug error occurs

988 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thucydides on Tue Apr 24 12:59:02 MST 2012
Hello,
Now I'm debugging LPC1343 via LPC-Link by using "Debug As" from LPCXpresso IDE (LPCXpresso_4.2.2_275).
But always a target error occurs.
The error dialog shows that

Reason:
15: Target error from set/break watch
Unable to set an execution break - no resource available.

Firstly the problem occurred for only par of projects but now I can't debug normally all of the projects.
When I used the LPCXpresso_4.1.5, i thought it's problem by version and I newly installed the LPCXpresso_4.2.2_275 but same as the old one.
I'll buy new LPC1343 and check if it's hardware problem or not.
If someone who experienced this problem, please write how to solve it.

Thanks,
0 项奖励
回复
2 回复数

908 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by steventso92 on Fri Feb 01 00:09:05 MST 2013
Get rid of the breakpoint, compile the program, program the program in (by debugging it), set breakpoints when you are able to press the 'Run' button under debugging.
0 项奖励
回复

908 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Apr 24 13:32:03 MST 2012
Did you read this already?

http://support.code-red-tech.com/CodeRedWiki/HowManyBreakpoints
0 项奖励
回复