Always LPC-Link error while initialization!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Always LPC-Link error while initialization!

1,597 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xpresso_1769 on Thu Apr 12 08:55:09 MST 2012
Hello,
I need help. I am trying to get my LPC-Link to work. It always hangs in the initialization process...

I tryed several things:
- new xpresso board
- different usb cabel
- reset bootloader via isp
- vector catch
- system restart
- different usb port

My system:
- win xp/ sp3
- notebook

During the diagnostic I get a missing winusb.dll message...

here the setupapi.log:


[SetupAPI Log]
Betriebssystemversion = 5.1.2600 Service Pack 3
Plattform-ID = 2 (NT)
Service Pack = 3.0
Suite = 0x0000
Produkttyp = 1
Architektur = x86
[2012/04/12 15:45:18 1132.2]
#-199 Executing "C:\WINDOWS\system32\rundll32.exe" with command line: rundll32.exe newdev.dll,ClientSideInstall \\.\pipe\PNP_Device_Install_Pipe_0.{9AFBE55B-37F3-4AB3-9F76-C7300A0BE094}
#I060 Set selected driver.
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#I022 Found "USB\VID_0471&PID_DF55" in C:\WINDOWS\inf\oem44.inf; Device: "USB Device with DFU Capabilities"; Driver: "USB Device with DFU Capabilities"; Provider: "Philips (NXP)"; Mfg: "Philips (NXP)"; Section name: "DFU.Dev".
#I087 Driver node not trusted, rank changed from 0x00000001 to 0x00008001.
#I023 Actual install section: [DFU.Dev.NTx86]. Rank: 0x00008001. Effective driver date: 03/11/2010.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#I063 Selected driver installs from section [DFU.Dev] in "c:\windows\inf\oem44.inf".
#I320 Class GUID of device remains: {36FC9E60-C465-11CF-8056-444553540000}.
#I060 Set selected driver.
#I058 Selected best compatible driver.
#I060 Set selected driver.
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#I022 Found "USB\VID_0471&PID_DF55" in C:\WINDOWS\inf\oem44.inf; Device: "USB Device with DFU Capabilities"; Driver: "USB Device with DFU Capabilities"; Provider: "Philips (NXP)"; Mfg: "Philips (NXP)"; Section name: "DFU.Dev".
#I087 Driver node not trusted, rank changed from 0x00000001 to 0x00008001.
#I023 Actual install section: [DFU.Dev.NTx86]. Rank: 0x00008001. Effective driver date: 03/11/2010.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#I063 Selected driver installs from section [DFU.Dev] in "c:\windows\inf\oem44.inf".
#I320 Class GUID of device remains: {36FC9E60-C465-11CF-8056-444553540000}.
#I060 Set selected driver.
#I058 Selected best compatible driver.
#-124 Doing copy-only install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2".
#W334 Failed to verify catalog when scanning file queue. Error 1168: Element nicht gefunden.
#E360 An unsigned or incorrectly signed file "c:\windows\inf\oem44.inf" for driver "USB Device with DFU Capabilities" will be installed (Policy=Ignore). Error 1168: Element nicht gefunden.
#W187 Install failed, attempting to restore original files.
#E360 An unsigned or incorrectly signed file "c:\windows\inf\oem44.inf" for driver "USB Device with DFU Capabilities" will be installed (Policy=Ignore). Error 1168: Element nicht gefunden.
#-024 Copying file "C:\nxp\lpcxpresso_3.6\Drivers\DFU\MassDfu.sys" to "C:\WINDOWS\system32\drivers\MassDfu.sys".
#E360 An unsigned or incorrectly signed file "C:\nxp\lpcxpresso_3.6\Drivers\DFU\MassDfu.sys" for driver "USB Device with DFU Capabilities" will be installed (Policy=Ignore). Error 1168: Element nicht gefunden.
#-166 Device install function: DIF_REGISTER_COINSTALLERS.
#I056 Coinstallers registered.
#-166 Device install function: DIF_INSTALLINTERFACES.
#-011 Installing section [DFU.Dev.NTx86.Interfaces] from "c:\windows\inf\oem44.inf".
#I054 Interfaces installed.
#-166 Device install function: DIF_INSTALLDEVICE.
#I123 Doing full install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2".
#I121 Device install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2" finished successfully.
[2012/04/12 16:10:35 5060.657]
#-198 Command line processed: "C:\WINDOWS\system32\mmc.exe" C:\WINDOWS\system32\devmgmt.msc /s 
#-166 Device install function: DIF_REMOVE.
#I289 Removing device "USB\VID_0471&PID_DF55\6&28E0277E&0&2".
#I048 Device removed.
[2012/04/12 16:10:44 676.163 Driver Install]
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#-198 Command line processed: C:\WINDOWS\system32\services.exe
#I022 Found "USB\VID_0471&PID_DF55" in C:\WINDOWS\inf\oem44.inf; Device: "USB Device with DFU Capabilities"; Driver: "USB Device with DFU Capabilities"; Provider: "Philips (NXP)"; Mfg: "Philips (NXP)"; Section name: "DFU.Dev".
#I087 Driver node not trusted, rank changed from 0x00000001 to 0x00008001.
#I023 Actual install section: [DFU.Dev.NTx86]. Rank: 0x00008001. Effective driver date: 03/11/2010.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#I063 Selected driver installs from section [DFU.Dev] in "c:\windows\inf\oem44.inf".
#I320 Class GUID of device remains: {36FC9E60-C465-11CF-8056-444553540000}.
#I060 Set selected driver.
#I058 Selected best compatible driver.
#-166 Device install function: DIF_INSTALLDEVICEFILES.
#I124 Doing copy-only install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2".
#-011 Installing section [DFU.Dev.NTx86] from "c:\windows\inf\oem44.inf".
#E358 An unsigned or incorrectly signed file "c:\windows\inf\oem44.inf" for driver "USB Device with DFU Capabilities" blocked (server install). Error 1168: Element nicht gefunden.
#E122 Device install failed. Error 1168: Element nicht gefunden.
#E157 Default installer failed. Error 1168: Element nicht gefunden.
[2012/04/12 16:10:48 3600.2]
#-199 Executing "C:\WINDOWS\system32\rundll32.exe" with command line: rundll32.exe newdev.dll,ClientSideInstall \\.\pipe\PNP_Device_Install_Pipe_0.{B1E6B306-04FB-4BCD-8528-AD9A132E6CA3}
#I060 Set selected driver.
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#I022 Found "USB\VID_0471&PID_DF55" in C:\WINDOWS\inf\oem44.inf; Device: "USB Device with DFU Capabilities"; Driver: "USB Device with DFU Capabilities"; Provider: "Philips (NXP)"; Mfg: "Philips (NXP)"; Section name: "DFU.Dev".
#I087 Driver node not trusted, rank changed from 0x00000001 to 0x00008001.
#I023 Actual install section: [DFU.Dev.NTx86]. Rank: 0x00008001. Effective driver date: 03/11/2010.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#I063 Selected driver installs from section [DFU.Dev] in "c:\windows\inf\oem44.inf".
#I320 Class GUID of device remains: {36FC9E60-C465-11CF-8056-444553540000}.
#I060 Set selected driver.
#I058 Selected best compatible driver.
#I060 Set selected driver.
#-019 Searching for hardware ID(s): usb\vid_0471&pid_df55&rev_0001,usb\vid_0471&pid_df55
#-018 Searching for compatible ID(s): usb\class_fe&subclass_01&prot_00,usb\class_fe&subclass_01,usb\class_fe
#I022 Found "USB\VID_0471&PID_DF55" in C:\WINDOWS\inf\oem44.inf; Device: "USB Device with DFU Capabilities"; Driver: "USB Device with DFU Capabilities"; Provider: "Philips (NXP)"; Mfg: "Philips (NXP)"; Section name: "DFU.Dev".
#I087 Driver node not trusted, rank changed from 0x00000001 to 0x00008001.
#I023 Actual install section: [DFU.Dev.NTx86]. Rank: 0x00008001. Effective driver date: 03/11/2010.
#-166 Device install function: DIF_SELECTBESTCOMPATDRV.
#I063 Selected driver installs from section [DFU.Dev] in "c:\windows\inf\oem44.inf".
#I320 Class GUID of device remains: {36FC9E60-C465-11CF-8056-444553540000}.
#I060 Set selected driver.
#I058 Selected best compatible driver.
#-124 Doing copy-only install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2".
#W334 Failed to verify catalog when scanning file queue. Error 1168: Element nicht gefunden.
#E360 An unsigned or incorrectly signed file "c:\windows\inf\oem44.inf" for driver "USB Device with DFU Capabilities" will be installed (Policy=Ignore). Error 1168: Element nicht gefunden.
#W187 Install failed, attempting to restore original files.
#E360 An unsigned or incorrectly signed file "c:\windows\inf\oem44.inf" for driver "USB Device with DFU Capabilities" will be installed (Policy=Ignore). Error 1168: Element nicht gefunden.
#-024 Copying file "C:\nxp\LPCXpresso_4.2.2_275\Drivers\DFU\MassDfu.sys" to "C:\WINDOWS\system32\drivers\MassDfu.sys".
#E360 An unsigned or incorrectly signed file "C:\nxp\LPCXpresso_4.2.2_275\Drivers\DFU\MassDfu.sys" for driver "USB Device with DFU Capabilities" will be installed (Policy=Ignore). Error 1168: Element nicht gefunden.
#-166 Device install function: DIF_REGISTER_COINSTALLERS.
#I056 Coinstallers registered.
#-166 Device install function: DIF_INSTALLINTERFACES.
#-011 Installing section [DFU.Dev.NTx86.Interfaces] from "c:\windows\inf\oem44.inf".
#I054 Interfaces installed.
#-166 Device install function: DIF_INSTALLDEVICE.
#I123 Doing full install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2".
#I121 Device install of "USB\VID_0471&PID_DF55\6&28E0277E&0&2" finished successfully.
 


Thanks in advance,
0 项奖励
回复
4 回复数

1,527 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xpresso_1769 on Fri Apr 13 05:12:22 MST 2012
I tried xpresso on several other systems like win7 64bit desktop, win xp sp2 notebook, win xp sp2 desktop.
I have never had any problems with xpresso....

What should I do with this two files?
0 项奖励
回复

1,527 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Apr 13 04:39:00 MST 2012
I've never seen this error (installed LPCXpresso on a lot XP/SP3 machines and laptops already without problems), but it seems to be a windows problem.

So it could be a good idea to remove LPCXpresso and install it again. Did you receive a message from firewall or antivir program?

Also it could be a good idea to check files mentioned in  c:\windows\inf\oem44.inf like %10%\system32\drivers\MassDfu.sys :)
0 项奖励
回复

1,527 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xpresso_1769 on Fri Apr 13 03:09:15 MST 2012
Thanks Zero for the quick answer, but it doesn't work.
Do you have another idea?

I forgot to mention that I just tried the manual fix! The other tools require a registration...
0 项奖励
回复

1,527 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Apr 12 10:01:25 MST 2012

Quote:

Typically, the [B][COLOR=DarkRed]Error 1168[/COLOR][/B] Element Not Found error message is caused by  Microsoft Windows system  malfunction. Damaged system data files are  usually a substantial danger to the overall health of a laptop or  desktop.

See: http://www.pcmmc.com/error-1168-element-not-found.php
0 项奖励
回复