Adding emWin do LPC project and C++ application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding emWin do LPC project and C++ application

756 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by littlejohn on Thu Apr 09 06:26:47 MST 2015
Hello,


I have problem with adding emWin library do my LPCXpresso project. I have read emWin documentation, but I still don't know.
Please give mi advice in order what I should to do.
I would like to add emWin to my project, create window and in this window show applicaion wrtitten in C++.
Then done application upload do Cortex M4. From what I can start?

Best regards :)
0 Kudos
Reply
1 Reply

642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Thu Apr 09 14:09:00 MST 2015
Hello Littlejohh,

I see that NXP does not have an easy to find overview of how to add emWin to a project - sorry about that! 

Please download the LPCOpen package for Keil MCB 1857 or Keil MCB 4357 [These are the only boards that has LCD built into and will support emWin without add on LCD modules] and import “emWin [emWin library placeholder project]”, “emwin_hello_world [Hello World example]” and “emwin_with_touch [Touch Screen example]” along with the board and chip libraries.
Inside the emWin project there is a “installation.txt” file that explains how to install the emwin libraries into the project area.

Best regards,
-NXP Support
0 Kudos
Reply