ARM7 Debug options using LPCXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ARM7 Debug options using LPCXpresso

675件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leojose on Mon Nov 18 00:51:01 MST 2013
It is clear that LPCLink2 will not support ARM7 or ARM9  -http://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-support

Although not mentioned anywhere, I assume the older LPCLink also does not support ARM7 and ARM9

But LPCXpresso IDE v6 supports ARM7/9, but it only support LPCLink debuggers.

So what are the options for somebody who wants to use LPCXpresso as an IDE for ARM7/ARM9?

LPCXPresso IDE -> ?Debugger? -> ARM7/9


0 件の賞賛
返信
1 返信

646件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Nov 18 01:25:17 MST 2013
For ARM7/9 debug with the LPCXpresso IDE, you need to either use the original LPC-Link (ie a separated LPCXpresso board) or a Red Probe+.

Regards,
LPCXpresso Support
0 件の賞賛
返信