AC Dimmer + lpc1114

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AC Dimmer + lpc1114

2,044 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hcanova on Sun Sep 01 18:26:15 MST 2013
Dear,

I'm trying to use the lpcxpresso 1114 to make an simple AC dimmer (in future I want to control it with CAN), basic I have an zero cross circuit connected to an interruption, this interruption will wait some time (to achieve the desired phase angle) and active an triac for certain amount of time, usually one pulse with few microseconds, my code for test is very simple, I'm trying to use the 32 bit timer to obtain the microsecond delay, but the ac load (in this case a light bulb), only blinks without fade effect, some one can share experiences whit this kind of circuit?


void PIOINT2_IRQHandler(void)
{
  uint32_t regVal;
  regVal = GPIOIntStatus( PORT2, 1 );
  if ( regVal )
  {
GPIOIntClear( PORT2, 1 );
  }

    delay32Ms(5000); // time to achieve the angle // 180º = 8333 microseconds // 60 hz
    GPIOSetValue( TRIAC_PORT, TRIAC_BIT, 1 ); 
    delay32Ms(10); // hit the triac for 10 microseconds
    GPIOSetValue( TRIAC_PORT, TRIAC_BIT,  0); 

  return;
}

Regards,
HCanova 
0 项奖励
回复
5 回复数

2,011 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hcanova on Mon Sep 02 17:49:20 MST 2013
Hi,

this is my timer code,
 LPC_SYSCON->SYSAHBCLKCTRL |=  0x00000400;


void delay32Ms( uint32_t delayInMs)
{

uint32_t test;

    LPC_TMR32B1->TCR = 0x02;/* reset timer */
    LPC_TMR32B1->PR  = 0x00;/* set prescaler to zero */

 

    LPC_TMR32B1->MR0 = delayInMs * ((SystemCoreClock/LPC_SYSCON->SYSAHBCLKDIV) / 1000000); 


    LPC_TMR32B1->IR  = 0xff;/* reset all interrrupts */
    LPC_TMR32B1->MCR = 0x04;/* stop timer on match */

    LPC_TMR32B1->TCR = 0x01;/* start timer */
  
    /* wait until delay time has elapsed */

    while (LPC_TMR32B1->TCR & 0x01);


  return;
}



I'will try to scope the output, but I need to find (or buy) one oscilloscope

thanks
0 项奖励
回复

2,011 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Mon Sep 02 05:20:23 MST 2013
And you have enabled SYSAHBCLKCTRL?
Please scope the clkout pin of your controller to see if the internal timings are correct.
For clkout pin configuration read sections 3.5.21, 3.5.22 en 3.5.23 of user manual 10398
0 项奖励
回复

2,011 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hcanova on Mon Sep 02 04:32:23 MST 2013
Sorry

I modified the function to obtain microsecond delay, but didn't changed the name, basic the MR0 of the timer is sysclock/1000000.
in this case 48000000/1000000 * delay

thanks
0 项奖励
回复

2,011 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hcanova on Mon Sep 02 04:30:19 MST 2013

Quote: serge
Is delay32Ms(xx) milliseconds or microseconds?
And are you sure?




Sorry, I modified the function to obtain microseconds delay, but I didn't changed the name, basic the MR0 of the timer is sysclock/1000000 (48000000/1000000)

Thanks
0 项奖励
回复

2,011 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Mon Sep 02 04:20:28 MST 2013
Is delay32Ms(xx) milliseconds or microseconds?
And are you sure?
0 项奖励
回复