8 bits vs. 32 bits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8 bits vs. 32 bits

1,374 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Sun Apr 24 12:57:23 MST 2011
Hi!

I want to introduce my last two jobs with microcontrollers.

The contract was to replace relays in silicon technology, and make them more animated signs (not just tic-tac).

The first one used old technology of 8 bits (MCS-51/AT89C4051):
http://www.youtube.com/watch?v=uFcg1spjSt8

In the second we use a modern LPC1111, and we can reduce consumption of 288 watts to just about 12 watts:
http://www.youtube.com/watch?v=vWRJR_KhVjE

My blog: http://luisdigital.blogspot.com

Thanks for watching me.
0 Kudos
Reply
4 Replies

1,364 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Mon Apr 25 10:52:13 MST 2011
Hi Luis,

I borrowed this from your blog.


Quote:
[COLOR=#0F0F5F]Above the sign consumed about 288 Watts, that's like having a blender lit 24 hours, which is very expensive to pay the electricity bill each month. [/COLOR]Now, with our advanced technology the sign only consumed about 12 Watts, so it consumes about your Internet modem.



You also need to pulse modulate the blender to get it's power consumption down.  It will make it cheaper to prepare the Piña coladas.  You can make them multicolor too and not so boring blanco.

Good job.

Larry
0 Kudos
Reply

1,364 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Mon Apr 25 10:50:21 MST 2011
Hello Luis,

Interesting project! :)

Other possibility: use the [FONT=Calibri]LPC11C24. This controller is cheap.  Direct coupling via CAN bus can easily be designed. Use on one pcb a separate controller and the possibilties are infinite.  Pcb-to-pcb wiring is simple: power + CAN.[/FONT]
[FONT=Calibri][/FONT]
[FONT=Calibri]The LPC11C24 is already realeased.[/FONT]
0 Kudos
Reply

1,364 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Mon Apr 25 08:59:32 MST 2011
Has implemented a PWM function to fade the letters but was not part of the order and was not used.

Also had a small problem is that the LEDs are not completely dimmed. Possibly due to the resistance in Pull-Up. Tomorrow will investigate this problem with my new board. :)
0 Kudos
Reply

1,365 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Mon Apr 25 01:29:16 MST 2011
Hello Luis,

well done!

[B]Every watt[/B] extra, will cost you per year a [B]few[/B] dollars ... your improvement will save you a lot of money.

Using transistors i.s.o. relays will open the possibility of using PWM and multicolor.
0 Kudos
Reply