7.5.0 -> 7.7.2 unable to program flash in LPC1114FN/102

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

7.5.0 -> 7.7.2 unable to program flash in LPC1114FN/102

1,220 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rdrosenber on Fri May 01 19:10:00 MST 2015
I just upgraded from 7.5.0 to 7.7.2.  Loading and debugging programs on LPC1114FN/102 in a custom hardware board works fine with 7.5.0.  After upgrading to 7.7.2, I cannot program the flash nor load/debug a program.


Log 7.7.2 for load/debug:
LPCXpresso RedlinkMulti Driver v7.7 (Mar 31 2015 21:02:36 - crt_emu_cm_redlink build 317)
Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
loaded v.2 On-chip Flash Memory LPC11_12_13_32K_4K.cfx
image 'LPC11_12_13 (32K Flash, min 4K RAM) Mar 17 2015 09:28:32'
Connected: was_reset=false. was_stopped=false
LPCXpresso Free License - Download limit is 256K
Writing 14948 bytes to address 0x00000000 in Flash
Target error from Commit Flash write: Em(12). System rejected access at location 0x10000AE4 - verify Population of memory and peripherals
(crt_emu_cm_redlink) terminating due to request from GDB


Log 7.7.2 for program flash:
Ni: LPCXpresso RedlinkMulti Driver v7.7 (Mar 31 2015 21:02:36 - crt_emu_cm_redlink build 317)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Xl:
Xc:
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Nc: loaded v.2 On-chip Flash Memory LPC11_12_13_32K_4K.cfx
Nc: image 'LPC11_12_13 (32K Flash, min 4K RAM) Mar 17 2015 09:28:32'
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=false
Cr:v LPCXpresso Free License - Download limit is 256K
Pc: ( 70) License Check Complete
Nt: Loading ELF file 'Serial_Port_Relay_Control_CmdI.axf' at location 00000000
Nt: Writing 14948 bytes to address 0x00000000 in Flash
Pb: 1 of 1 (  0) Writing pages 0-3 at 0x00000000 with 14948 bytes
Ps: (  0) at 00000000: 0 bytes - 0/14948
Pb: (100) Writing Flash ended with an error.
Ed:05: File 'Serial_Port_Relay_Control_CmdI.axf' load failure: Em(12). System rejected access at location 0x10000BF0 - verify Population of memory and peripherals
Pc: (100) Target Connection Failed


Log 7.5.0 for load/debug:
LPCXpresso RedlinkMulti Driver v7.5 (Oct 24 2014 22:18:51 - crt_emu_cm_redlink build 172)
Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Loaded LPC11_12_13_32K_4K.cfx: LPC11_12_13 (32K Flash, min 4K RAM) Oct 13 2014 15:50:32  On-chip Flash Memory
Connected: was_reset=false. was_stopped=true
v LPCXpresso Free License - Download limit is 256K
Writing 14824 bytes to address 0x00000000 in Flash
Erased/Wrote page  0-3 with 14824 bytes in 3406msec
Flash Write Done
Flash Program Summary: 14824 bytes in 3.41 seconds (4.25 KB/sec)
Stopped (Was Reset)  [Reset from Unknown]
Stopped: Breakpoint #1


Log 7.5.0 for program flash operation:
Ni: LPCXpresso RedlinkMulti Driver v7.5 (Oct 24 2014 22:18:51 - crt_emu_cm_redlink build 172)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Nc: Loaded LPC11_12_13_32K_4K.cfx: LPC11_12_13 (32K Flash, min 4K RAM) Oct 13 2014 15:50:32  On-chip Flash Memory

Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=false
Cr:v LPCXpresso Free License - Download limit is 256K
Pc: ( 70) License Check Complete
Nt: Loading ELF file 'Serial_Port_Relay_Control_CmdI.axf' at location 00000000
Nt: Writing 14824 bytes to address 0x00000000 in Flash
Pb: 1 of 1 (  0) Writing pages 0-3 at 0x00000000 with 14824 bytes
Ps: (  0) Page  0 at 00000000
Ps: (  0) Page  0 at 00000000: 2048 bytes
Ps: ( 13) Page  0 at 00000800: 2048 bytes
Ps: ( 27) Page  1 at 00001000: 2048 bytes
Ps: ( 41) Page  1 at 00001800: 2048 bytes
Ps: ( 55) Page  2 at 00002000: 2048 bytes
Ps: ( 69) Page  2 at 00002800: 2048 bytes
Ps: ( 82) Page  3 at 00003000: 2048 bytes
Ps: ( 96) Page  3 at 00003800: 488 bytes
Nt: Erased/Wrote page  0-3 with 14824 bytes in 3412msec
Pb: (100) Finished writing Flash successfully.
Nt: Flash Write Done


Thanks,
Rob
0 项奖励
回复
7 回复数

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rdrosenber on Sat May 23 18:55:40 MST 2015
OK, thanks for the explanation. 

The LPC-Link2 seemed to work with my target only if JP2 was installed even though my target was supplying power to what I thought was the VTref pin.  I discovered that my problem with needing JP2 connected was because I was providing target power to pin 1 of J6 (the LPCXpresso JTAG header).  Based on the schematics for the LPC-Link2, pin 1 on this connector is not the same as pin 1 on J7 and J8.  Instead of connecting my target power to J6 pin 1, I had to remove JP2 and connect the target power to pin 1 of JP2.  This provided target power to the LPC-Link2 buffers.

Yes, I am using the Redlink debug probe firmware.

Everything seems to be working well now.  Thank you for your help.
0 项奖励
回复

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed May 13 00:07:24 MST 2015
The original LPC-Link1 only supported 3.3V and did not get VTref from the target.  However the LPC-Link2 uses dual-supply buffers that allows it to work with targets using a different voltage (between 1.8V - 4.3V). 

On the LPC-Link2 board JP2 shunted will power the target side of the dual-supply buffer and provide power to the target through a diode on VTref.  With JP2 open the Target must supply the VTref to power the Target side of the dual-supply buffer.

We'll update our documentation to better reflect the above.

So far we haven't managed to identify any reason as to why you should see different behaviour between LPCXpresso 7.5.0 and 7.7.2 though. Just to confirm, you are using Redlink debug probe firmware soft-loaded by LPCXpresso when it first starts a debug session, rather than CMSIS-DAP firmware preprogrammed into the flash?

Regards,
LPCXpresso Support
0 项奖励
回复

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rdrosenber on Sun May 10 19:39:44 MST 2015
I reduced the hardware circuit to just the LPC1114FN28, a 3.3V voltage regulator and a LPC-Link debugger.  The LPC-Link debugger was connected to the LPC1114FN28 using a minimal SWD connection (SWDIO, SWDCLK, Reset, Ground).

When I used an original LPC-Link debugger (first generation, part of an LPCXpresso 1114 board), both versions of LPCXpresso were able to flash a program without errors.

When I used a LPC-Link2 debugger, LPCXpresso 7.5 programmed the flash without errors but LPCXpresso 7.7.2 failed with errors as shown in the logs of previous posts.

The LPC-Link2 pod with LPCXpresso 7.7.2 started working once I added a connection from the debugger interface JTAG VREF pin to the circuit 3.3V supply voltage and installed jumper JP2 on the LPC-Link2.

After reading about the JTAG VREF pin and examining the schematic for the LPC-Link2, I understand the need for this connection.  I do not understand why the LPC-Link2 worked with previous versions of LPCXpresso without the JTAG VREF connection installed.  Any insight would be useful.

Thank you for your prompt aid in trying to troubleshoot this problem.
0 项奖励
回复

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun May 03 01:44:06 MST 2015
Thank you for your logs. In order for us to investigate further please can you confirm if you can successfully launch a debug session if you boot your board into ISP mode first?

Also, after mass erasing the part does the next debug session program the flash and start correctly?

It would also be interesting if you could try programming a different image a few times (after mass erasing first), and seeing if you see the same behaviour.

Finally is there any chance of getting your application project - buildable with sources if possible, else at least the AXF and linker map file - so that we can try to reproduce the problem here?

Regards,
LPCXpresso Support
0 项奖励
回复

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rdrosenber on Sat May 02 14:34:31 MST 2015
I was able to use an LPC-Link2 debugger connected to the SWD pins on the LPC1114 and LPCXpresso 7.7.2 to mass erase the flash of the microcontroller as the following log shows.

Ni: LPCXpresso RedlinkMulti Driver v7.7 (Mar 31 2015 21:02:36 - crt_emu_cm_redlink build 317)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Nc: loaded v.2 On-chip Flash Memory LPC11_12_13_32K_4K.cfx
Nc: image 'LPC11_12_13 (32K Flash, min 4K RAM) Mar 17 2015 09:28:32'
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=true
Cr:v LPCXpresso Free License - Download limit is 256K
Pc: ( 70) License Check Complete
Nt: Mass Erase
Nt: MassErase completed (in 111ms)


I set the following: "Extended debug trace (DEBUG_TRACE)" to 4095

Debug log with vector catch set to False:
LPCXpresso RedlinkMulti Driver v7.7 (Mar 31 2015 21:02:36 - crt_emu_cm_redlink build 317)
Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
loaded v.2 On-chip Flash Memory LPC11_12_13_32K_4K.cfx
image 'LPC11_12_13 (32K Flash, min 4K RAM) Mar 17 2015 09:28:32'
Non-default CRT_DEBUG_TRACE set (to 0xFFF)
Driver 'page' size 2048 (0x800) cache size 2048 (0x800)
(Driver has verify, fast erase multiple, chip erase, verifies on program)
(allow background transfers, erase sector quantum 0xFFFFFFFF)
Connected: was_reset=false. was_stopped=true
LPCXpresso Free License - Download limit is 256K
FlashStart
FLASH algorithm download complete (at 0x10000000 888 bytes)
BEFORE execution
Driver Register State
R0:     10000C38
R1:     00000000
R2:     00000000
R3:     00000000
R4:     00000000
R5:     00000000
R6:     00000000
R7:     00000000
R8:     00000000
R9:     00000000
R10:    00000000
R11:    00000000
R12:    00000000
SP:     10000438
LR:     10000035
PC:     10000034
xPSR:   01000000
MSP:    10000438
PSP:    10000438
started processor at 0x10000035 (stack at 0x10000438 mail at 0x10000C38)
Flash Driver V.2 startup - OK
FLASH driver initialization complete - rc OK
Writing 17564 bytes to address 0x00000000 in Flash
FlashProgram at 0x0[0x449C] verify erasing
0[0x449C] flashing block - buf 0x960c0f8
Chan for 0x449c bytes, cache 1 x 0x800 @0x10000438
(  0) at 00000000: 0 bytes - 0/17564
00000000[0x449C] erase flash
10000C38: v.2 cmd 0008 (EraseSector) param [00000000, 00000000, 00000005]
op EraseSector starting
10000438[0x800] written - 10001000 00000149 000001CD 000001D5 ... [512 words in 46 ms ~44kBps] - rc Em(12). System rejected access at location 0x10000984 - verify Population of memory and peripherals
10000438[0x800] chan sending #0 written #0/9 - rc Em(12). System rejected access at location 0x10000984 - verify Population of memory and peripherals
op EraseSector total wait was 51 ms
(v2) op #0x8 EraseSector(0x0, 0x0, 0x5) Failed - rc Em(12). System rejected access at location 0x10000984 - verify Population of memory and peripherals
Chan end 0x449c bytes left
Chan after 0x449C bytes 0 ms unused transfer time
FlashEnd
10000C38: v.2 cmd 0100 (Terminate) param [00000000, 00000000, 00000000]
op Terminate starting
op Terminate cmd 0x100 status 0x0 wait 17/500 ms
op Terminate total wait was 17 ms
(v2) op #0x100 Terminate(0x0, 0x0, 0x0) OK - rc OK
Halted processor (rc OK)
Target error from Commit Flash write: Em(12). System rejected access at location 0x10000984 - verify Population of memory and peripherals
(crt_emu_cm_redlink) terminating due to request from GDB
Flash object destroyed


Performed flash mass erase again successfully.

Debug log with vector catch set to True:
LPCXpresso RedlinkMulti Driver v7.7 (Mar 31 2015 21:02:36 - crt_emu_cm_redlink build 317)
Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Enabled.
loaded v.2 On-chip Flash Memory LPC11_12_13_32K_4K.cfx
image 'LPC11_12_13 (32K Flash, min 4K RAM) Mar 17 2015 09:28:32'
Non-default CRT_DEBUG_TRACE set (to 0xFFF)
Driver 'page' size 2048 (0x800) cache size 2048 (0x800)
(Driver has verify, fast erase multiple, chip erase, verifies on program)
(allow background transfers, erase sector quantum 0xFFFFFFFF)
Connected: was_reset=true. was_stopped=true
LPCXpresso Free License - Download limit is 256K
FlashStart
FLASH driver initialization failed - rc Em(12). System rejected access at location 0x100002F0 - verify Population of memory and peripherals
FlashEnd
10000C38: v.2 cmd 0100 (Terminate) param [00000000, 00000000, 00000000]
op Terminate starting
op Terminate cmd 0x100 status 0x0 wait 17/500 ms
op Terminate cmd 0x100 status 0x0 wait 35/500 ms
op Terminate cmd 0x100 status 0x0 wait 53/500 ms
op Terminate cmd 0x100 status 0x0 wait 72/500 ms
op Terminate cmd 0x100 status 0x0 wait 89/500 ms
op Terminate cmd 0x100 status 0x0 wait 108/500 ms
op Terminate cmd 0x100 status 0x0 wait 127/500 ms
op Terminate cmd 0x100 status 0x0 wait 145/500 ms
op Terminate cmd 0x100 status 0x0 wait 163/500 ms
op Terminate cmd 0x100 status 0x0 wait 182/500 ms
op Terminate cmd 0x100 status 0x0 wait 199/500 ms
op Terminate cmd 0x100 status 0x0 wait 217/500 ms
op Terminate cmd 0x100 status 0x0 wait 236/500 ms
op Terminate cmd 0x100 status 0x0 wait 254/500 ms
op Terminate cmd 0x100 status 0x0 wait 275/500 ms
op Terminate cmd 0x100 status 0x0 wait 292/500 ms
op Terminate cmd 0x100 status 0x0 wait 311/500 ms
op Terminate cmd 0x100 status 0x0 wait 328/500 ms
op Terminate cmd 0x100 status 0x0 wait 346/500 ms
op Terminate cmd 0x100 status 0x0 wait 362/500 ms
op Terminate cmd 0x100 status 0x0 wait 381/500 ms
op Terminate cmd 0x100 status 0x0 wait 399/500 ms
op Terminate cmd 0x100 status 0x0 wait 416/500 ms
op Terminate cmd 0x100 status 0x0 wait 437/500 ms
op Terminate cmd 0x100 status 0x0 wait 456/500 ms
op Terminate cmd 0x100 status 0x0 wait 475/500 ms
op Terminate cmd 0x100 status 0x0 wait 494/500 ms
op Terminate cmd 0x100 status 0x0 wait 512/500 ms
op Terminate total wait was 512 ms
Halted processor on op Terminate timeout
driver "Terminate" timeout (500 ms)  PC: 1FFF0040
Driver Register State
R0:     00000000
R1:     000004D9
R2:     000004D9
R3:     10000C14
R4:     40048000
R5:     EFFFEB15
R6:     40048000
R7:     10000F08
R8:     D9019A91
R9:     0F355205
R10:    2A187030
R11:    A14BC3D0
R12:    10000483
SP:     10000FFC
LR:     FFFFFFF9
PC:     1FFF0040
xPSR:   C1000000
MSP:    10000FFC
PSP:    36406280
10001018:  xPSR:   00000800
10001014:  VECTPC: 10000438
10001010:  LR:     00000378
1000100C:  R12:    10000000
10001008:  R3:     00001032
10001004:  R2:     54000045
10001000:  R1:     23010020
10000FFC:  R0:     1FFF10FF
BFAR:   00000000
CFSR:   00000000
HFSR:   00000000
DFSR:   00000000
AFSR:   00000000
reset reason -
Unknown
Driver Register State
R0:     00000000
R1:     000004D9
R2:     000004D9
R3:     10000C14
R4:     40048000
R5:     EFFFEB15
R6:     40048000
R7:     10000F08
R8:     D9019A91
R9:     0F355205
R10:    2A187030
R11:    A14BC3D0
R12:    10000483
SP:     10000FFC
LR:     FFFFFFF9
PC:     1FFF0040
xPSR:   C1000000
MSP:    10000FFC
PSP:    36406280
10001018:  xPSR:   00000800
10001014:  VECTPC: 10000438
10001010:  LR:     00000378
1000100C:  R12:    10000000
10001008:  R3:     00001032
10001004:  R2:     54000045
10001000:  R1:     23010020
10000FFC:  R0:     1FFF10FF
BFAR:   00000000
CFSR:   00000000
HFSR:   00000000
DFSR:   00000000
AFSR:   00000000
(v2) op #0x100 Terminate(0x0, 0x0, 0x0) Failed - rc Ec: Flash driver "Terminate" timeout (500 ms)  PC: 1FFF0040
(100) Writing Flash ended with an error.
Target error from Commit Flash write: Em(12). System rejected access at location 0x100002F0 - verify Population of memory and peripherals


Sometimes I get failures performing the flash mass erase as well:
Ni: LPCXpresso RedlinkMulti Driver v7.7 (Mar 31 2015 21:02:36 - crt_emu_cm_redlink build 317)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Nc: loaded v.2 On-chip Flash Memory LPC11_12_13_32K_4K.cfx
Nc: image 'LPC11_12_13 (32K Flash, min 4K RAM) Mar 17 2015 09:28:32'
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=true. was_stopped=false
Cr:v LPCXpresso Free License - Download limit is 256K
Pc: ( 70) License Check Complete
Nt: Mass Erase
Ed:04: Failed to erase flash: Em(12). System rejected access at location 0x1000032C - verify Population of memory and peripherals
Pc: (100) Target Connection Failed


All of these operations complete successfully using LPCXpresso 7.5.0

Debug log with vector catch set to False:
LPCXpresso RedlinkMulti Driver v7.5 (Oct 24 2014 22:18:51 - crt_emu_cm_redlink build 172)
Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Loaded LPC11_12_13_32K_4K.cfx: LPC11_12_13 (32K Flash, min 4K RAM) Oct 13 2014 15:50:32  On-chip Flash Memory
Connected: was_reset=false. was_stopped=true
v LPCXpresso Free License - Download limit is 256K
Writing 17564 bytes to address 0x00000000 in Flash
Erased/Wrote page  0-4 with 17564 bytes in 4105msec
Flash Write Done
Flash Program Summary: 17564 bytes in 4.11 seconds (4.18 KB/sec)
Stopped (Was Reset)  [Reset from Unknown]
Stopped: Breakpoint #1


Debug log with vector catch set to True:
LPCXpresso RedlinkMulti Driver v7.5 (Oct 24 2014 22:18:51 - crt_emu_cm_redlink build 172)
Emu(0): Conn&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Enabled.
Loaded LPC11_12_13_32K_4K.cfx: LPC11_12_13 (32K Flash, min 4K RAM) Oct 13 2014 15:50:32  On-chip Flash Memory
Connected: was_reset=true. was_stopped=true
v LPCXpresso Free License - Download limit is 256K
Writing 17564 bytes to address 0x00000000 in Flash
Erased/Wrote page  0-4 with 17564 bytes in 4348msec
Flash Write Done
Flash Program Summary: 17564 bytes in 4.35 seconds (3.94 KB/sec)
Stopped (Was Reset)  [Reset from Unknown]
Stopped: Breakpoint #1

0 项奖励
回复

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rdrosenber on Sat May 02 13:54:02 MST 2015
I will try the steps that you suggest; however the issue is not that the program cannot be debugged.  The issue seems to be a failure to properly program the flash memory on the LPC1114 based on the error messages of "Writing 14948 bytes to address 0x00000000 in Flash Target error from Commit Flash write: Em(12). System rejected access at location 0x10000AE4 - verify Population of memory and peripherals" and "Pb: 1 of 1 (  0) Writing pages 0-3 at 0x00000000 with 14948 bytes
Ps: (  0) at 00000000: 0 bytes - 0/14948
Pb: (100) Writing Flash ended with an error.
Ed:05: File 'Serial_Port_Relay_Control_CmdI.axf' load failure: Em(12). System rejected access at location 0x10000BF0 - verify Population of memory and peripherals"
0 项奖励
回复

1,052 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat May 02 04:42:36 MST 2015
It sounds like something in your image is putting the MCU into a state that is preventing the flash driver from taking control.

First of all, can you confirm if you can successfully launch a debug session if you boot your board into ISP mode first? This should prevent the code is flash being executed from reset.

Can you also see if there is any difference in behaviour seen if you enable "vector catch" functionality in the launch configuration.

http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
http://www.lpcware.com/content/faq/lpcxpresso/launch-configuration-menu

Please post debug logs from using LPCXpresso 7.7.2, both with vector catch enabled and without - ensuring that you first switch on the "DEBUG TRACE" option as follows:

* use the "Preferences..." dialogue:
* ensure the LPCXpresso group of options are expanded
* select the "Debug Options (Advanced)" choice
* fill in the box labelled "Extended debug trace (DEBUG_TRACE)" with 4095

http://www.lpcware.com/content/faq/lpcxpresso/debug-log

Regards,
LPCXpresso Support
0 项奖励
回复