15: Target error from Commit Flash write

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

15: Target error from Commit Flash write

2,853件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maxmel on Tue Dec 21 02:44:36 MST 2010
hi,
  have this error message   15: Target error from Commit Flash write
  Flash erase or write operation aborted.
what is the reason ? thank you

Br,
0 件の賞賛
返信
2 返答(返信)

2,680件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maxmel on Tue Dec 21 03:15:41 MST 2010
Which MCU are you trying to debug?  lpc1114

Are you connecting via the LPC-Link to the built-in MCU on the LPCXpresso board, or have you split the LPC-Link off and are connecting to your own board?
i use lpcxpresso board
Have you ever been able to successfully download to the board? If so, what changed before you started to see the problem? yes

Do you see this problem downloading your own application or with the examples? If it is your own application, then can you successfully download and run a "standard" LPCXPresso example application?
examples

Please can you copy and paste the MCU debug log from the console view of the LPCXpresso IDE into this thread. You may need to use the "Monitor" icon of the console view in order to select the MCU debug log as the log file to display.
no  because i close i  launch again lpcxpresso and now it's working
0 件の賞賛
返信

2,680件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Dec 21 02:57:59 MST 2010
Bit hard to reply without a lot more information! For example...

Which MCU are you trying to debug?

Are you connecting via the LPC-Link to the built-in MCU on the  LPCXpresso board, or have you split the LPC-Link off and are connecting  to your own board?

Have you ever been able to successfully download to the board? If so, what changed before you started to see the problem?

Do you see this problem downloading your own application or with the examples? If it is your own application, then can you successfully download and run a "standard" LPCXPresso example application?

Please can you copy and paste the MCU debug log from the console view of  the LPCXpresso IDE into this thread. You may need to use the "Monitor" icon  of the console view in order to select the MCU debug log as the log  file to display.

Regards,
CodeRedSupport
0 件の賞賛
返信