What toolchains are compatible with LPC-Link ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What toolchains are compatible with LPC-Link ?

2,603 Views
lpcware-support
Senior Contributor I

LPC-Link, the debug probe built into the original LPCXpresso board design, is only compatible with the LPCXpresso IDE (and the now discontinued Code Red Technologies Red Suite product).

If you want a debug probe suitable for use with another toolchain, such as Keil or IAR, then you should consider LPC-Link2 - either in standalone form or as built in to the LPCXpresso V2 boards.

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies