What toolchains are compatible with LPC-Link ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What toolchains are compatible with LPC-Link ?

2,583件の閲覧回数
lpcware-support
Senior Contributor I

LPC-Link, the debug probe built into the original LPCXpresso board design, is only compatible with the LPCXpresso IDE (and the now discontinued Code Red Technologies Red Suite product).

If you want a debug probe suitable for use with another toolchain, such as Keil or IAR, then you should consider LPC-Link2 - either in standalone form or as built in to the LPCXpresso V2 boards.

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)