53: License does not permit flash operations from the command line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

53: License does not permit flash operations from the command line

2,571件の閲覧回数
lpcware-support
Senior Contributor I

If you try to directly use the GUI flash programmer, or the command line flash programmer, but have not activated your LPCXpresso license, then you will see an error such as:

53: License does not permit flash operations from the command line

In such case, activating your copy of LPCXpresso should solve the problem.

If the LPCXpresso IDE indicates that you have activated, but you still see this problem, the the debug driver is failing to find your license. There are a number of reasons why this might happen. For details of how to solve such problems, please see the FAQ:

ラベル(2)
0 件の賞賛
返信
0 返答(返信)