will write?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

will write?

1,772 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nobuo kawano on Mon Aug 27 19:51:01 MST 2012
hi all Please tell me

I want to write to the FLASH memory from the CAN2.0 using LPC11C24
I want to know is whether you are compatible flashmagic.
Labels (1)
0 Kudos
Reply
3 Replies

1,760 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nobuo kawano on Wed Aug 29 18:22:39 MST 2012
Hello gentlemen

Did you need PEAK P-CAN USB CAN2.0 adapter also,
Us does not only have elm327 obd2 adapter,
I consider buying.

Thank you.
0 Kudos
Reply

1,760 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Aug 29 09:12:07 MST 2012
Chapter 26.6 C_CAN communication protocol of UM10398 LPC111x/LPC11Cxx User manual Rev. 11 — 26 July 2012 is describing C_CAN ISP SDO communication.
There's described which IDs are used to communicate with LPC11Cx4. So a 'raw data' bin file can be used to transmit it in 4k sectors.
This can be done by every LPC with CAN controller like LPC1768 or even a LPC11C14.  
0 Kudos
Reply

1,760 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjnbarrass on Wed Aug 29 02:41:36 MST 2012
Hello,

You need a recent Flash Magic version - available from:  http://www.flashmagictool.com/

Note: the flash magic tool only support CAN adapters from PEAK (Phytec) - so you will need P-CAN USB CAN2.0 adapter if you don't already have one.

I am also looking to program the LPC11C24 over CAN - but I also intend to do this from another embedded MCU (LPC18xx btw) over CAN... getting the protocol/CANopen dictionary is proving difficult.
0 Kudos
Reply