wifi module connect to lpc1769

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wifi module connect to lpc1769

1,562件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nang on Sun Aug 11 22:25:39 MST 2013
Hi I have question for lpc1769 to wifi ,now current time connect to Ethernet lan8720 that ok, but I need to change to wifi, some body's know solution or ic path or module please provide or detail .

thank you.
[email protected]
ラベル(1)
0 件の賞賛
返信
1 返信

1,208件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by usb10185 on Mon Aug 12 07:48:42 MST 2013
Most WiFi Radio chipsets will communicate to the micro via SPI or UART.
Do you want to run a stack on the LPC or expect the Wifi Module to run the stack? It depends if what you want really!

Check out mbed which uses NXP LPC1769 and LPC1100 parts: http://mbed.org/cookbook/Internet-of-things-using-Wifi
0 件の賞賛
返信