why the spinbox disable receive the input focus when use TAB key?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

why the spinbox disable receive the input focus when use TAB key?

911 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ling3wei on Mon Nov 19 21:36:29 MST 2012
why the spinbox disable receive the input focus when use TAB key?
I will be using a Spinbox widget without a touch or mouse interface, only using the,tab, up, down, left, right,enter,space keys of a keyboard. the other widget is able to receive the input foucs but the spinbox can`t.
My code :
static const GUI_WIDGET_CREATE_INFO _aDialogCreate[] = {
  { FRAMEWIN_CreateIndirect, "", ID_FRAMEWIN_0, 0, 35, 331, 328, 0, 0, 0 },
  { BUTTON_CreateIndirect, "", ID_BUTTON_0, 68, 225, 85, 50, 0, 0, 0 },
  { BUTTON_CreateIndirect, "", ID_BUTTON_1, 202, 225, 85, 50, 0, 0, 0 },
  { SPINBOX_CreateIndirect, "", GUI_ID_SPINBOX0_11, 2, 2, 65, 40, 0, 0, 0 },
};
标签 (1)
0 项奖励
回复
0 回复数