where to get GUI Builder?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where to get GUI Builder?

4,328 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kada on Fri Dec 21 10:11:16 MST 2012
the Segger emWin website describes the "GUI Builder" application, a way to automatically generate code for emWin from a graphical editor.  I contacted the Segger support, and he said that NXP users can get this for free thru NXP/LPCware.  Can anyone point me to where I can get GUI Builder from?
Labels (1)
0 Kudos
Reply
5 Replies

3,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Cusko on Thu Feb 14 05:08:10 MST 2013
The GUI_Builder is not an advanced tool. It is useful for positioning the elements and that's about it.
0 Kudos
Reply

3,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by studyembedded on Thu Feb 14 03:05:44 MST 2013
I am sure it is bundled with emWin pack...or check tutorial on www.zembedded.com best of luck!
0 Kudos
Reply

3,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kada on Fri Dec 21 15:12:40 MST 2012
THANKS!!!
0 Kudos
Reply

3,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Dec 21 12:51:00 MST 2012
Please install latest version of BSP with latest emWin library version 5.18 from
http://www.lpcware.com/content/nxpfile/segger-emWin-518-libraries-nxp-mcus-version-100-0


After installation you can find GUI Builder in the below folder.
..\NXP_emWin518_BSP\Start\Tools

---------
Thanks,
NXP Support
0 Kudos
Reply

3,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DF9DQ on Fri Dec 21 10:15:22 MST 2012
Download and install one of the BSPs from here:
http://www.lpcware.com/content/project/emwin-graphics-library
This will also install GUIBuilder.

Regards,
Rolf
0 Kudos
Reply