what is "c_entry" for?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is "c_entry" for?

1,858 Views
hosseinef
Contributor II

Hi, 

I am new to LPC MCUs programming. In an example i encountered to using of "c_entry" function in the code. Whats that for? 

regards

0 Kudos
Reply
2 Replies

1,739 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I suspect that you are looking at some very old example code => at one point in time, various toolchains used a function called "c_entry" as their main user application code entry point, which would be called from the startup code (rather than the "main" function).

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

1,739 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please mention the device and software you are using?

Regards

Sol

0 Kudos
Reply