waveshare

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

waveshare

1,976件の閲覧回数
steverobinson
Contributor I

example code

0 件の賞賛
返信
2 返答(返信)

1,917件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Steve,

Can you tell me the processor part number you are using? Anyway, for LPC family, if you use LPC54xxx or LPC8xx, you can use SDK, which can be downloaded from the link:

MCUXpresso SDK|NXP 

If you use the other family, you can consider to use LPCOPEN from the link:

LPCOpen Libraries and Examples|NXP 

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信

1,917件の閲覧回数
steverobinson
Contributor I

Xiangjun Rong

Thanks for pointing me to the LPCOPEN site.

I found there the AN11771 which describes connecting LPC82x with a 2.9

inch epaper display.

I have the 4.2 inch epaper display from Waveshare which has different

registers. And, I am using LPC1768 to drive it.

I had hoped someone had been 'down this route' to save me time. But,

I'll get there:)

Thanks again

steve robinson

0 件の賞賛
返信