waveshare

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

waveshare

1,976 Views
steverobinson
Contributor I

example code

0 Kudos
Reply
2 Replies

1,917 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Steve,

Can you tell me the processor part number you are using? Anyway, for LPC family, if you use LPC54xxx or LPC8xx, you can use SDK, which can be downloaded from the link:

MCUXpresso SDK|NXP 

If you use the other family, you can consider to use LPCOPEN from the link:

LPCOpen Libraries and Examples|NXP 

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

1,917 Views
steverobinson
Contributor I

Xiangjun Rong

Thanks for pointing me to the LPCOPEN site.

I found there the AN11771 which describes connecting LPC82x with a 2.9

inch epaper display.

I have the 4.2 inch epaper display from Waveshare which has different

registers. And, I am using LPC1768 to drive it.

I had hoped someone had been 'down this route' to save me time. But,

I'll get there:)

Thanks again

steve robinson

0 Kudos
Reply