vcom baud setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vcom baud setting

1,728 Views
kensu
Contributor V

Hello,

I use the "usbd_rom_cdc_vcom" sample project, it works good. But I want to change the baudrate to 9600 (now is 115200)

Could someone tell me how to change the bard rate setting for NXP1830 virtual com port?

Where the source code to modify?

Thanks

Ken

Labels (2)
Tags (2)
1 Reply

1,504 Views
soledad
NXP Employee
NXP Employee

Hi,

You can change the baudrate in the board.c file. After change the value rebuild the "usbd_rom_cdc_vcom" project.

pastedImage_1.png

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------