vcom baud setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vcom baud setting

1,701件の閲覧回数
kensu
Contributor V

Hello,

I use the "usbd_rom_cdc_vcom" sample project, it works good. But I want to change the baudrate to 9600 (now is 115200)

Could someone tell me how to change the bard rate setting for NXP1830 virtual com port?

Where the source code to modify?

Thanks

Ken

ラベル(2)
タグ(2)
1 返信

1,477件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

You can change the baudrate in the board.c file. After change the value rebuild the "usbd_rom_cdc_vcom" project.

pastedImage_1.png

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------