vant burn code on my controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vant burn code on my controller

1,227件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by naveed_33 on Mon Dec 31 06:26:55 MST 2012
Hello,
i am using lpc 1857(MCB 1857 eval board) microcontroller. i have tried burning my code on it with jlink and u link. but it gives the following error (on attolic studio)
ERROR: Could not power up debug port: Control/Status register reads 00000041
ERROR: Can not read register 0 (R0) while CPU is running

ERROR: Can not read register 1 (R1) while CPU is running

ERROR: Can not read register 2 (R2) while CPU is running

ERROR: Can not read register 3 (R3) while CPU is running

ERROR: Can not read register 4 (R4) while CPU is running

ERROR: Can not read register 5 (R5) while CPU is running

ERROR: Can not read register 6 (R6) while CPU is running

ERROR: Can not read register 7 (R7) while CPU is running

ERROR: Can not read register 8 (R8) while CPU is running

ERROR: Can not read register 9 (R9) while CPU is running

ERROR: Can not read register 10 (R10) while CPU is running

ERROR: Can not read register 11 (R11) while CPU is running

ERROR: Can not read register 12 (R12) while CPU is running

ERROR: Can not read register 13 (R13) while CPU is running

ERROR: Can not read register 14 (R14) while CPU is running

ERROR: Can not read register 15 (R15) while CPU is running

ERROR: Can not read register 16 (XPSR) while CPU is running
ラベル(1)
0 件の賞賛
返信
1 返信

1,213件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Fri Jan 11 17:12:28 MST 2013
Hi naveed_33,

The LPC18xx is in the Atollic supported devices list here:
http://www.atollic.com/index.php/targets/armtargetsupport/nxp-lpc
so it should work.

Technical support is available at these two addresses:

Technical support in Europe and world-wide:
[email protected]
Technical support in North, Central and South america:
[email protected]

-Dave @ NXP
0 件の賞賛
返信