using feedback register for mcpwm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using feedback register for mcpwm

1,687件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by praveenb on Wed Mar 11 03:32:38 MST 2015
HI anyone knows about using feedback register of MCPWM, i am not getting how to use please help
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,649件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by praveenb on Sat Mar 14 02:08:26 MST 2015


Hi Thanks for replaying

That coder is for DC motor, but i need for AC motor

i am using MCPWM to generate signal having 90 degree phase shift in AC mode, to check the signal either it is +ve and -ve direction, i used the QEI module to check the direction, it showing direction and phase error,to remove that error what have to do?,i thought feedback register can solve that problem

I generated the signal as given in the Fig 130.Quadrature Encoder Basic Operation of UM10360
i am using only 2 signal Pha and Phb
0 件の賞賛
返信

1,649件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by praveenb on Fri Mar 13 22:22:15 MST 2015
Hi Thanks for replaying

That coder is for DC motor, but i need for AC motor

i am using MCPWM to generate signal having 90 degree phase shift in AC mode, to check the signal either it is +ve and -ve direction, i used the QEI module to check the direction, it showing direction and phase error,to remove that error what have to do?,i thought feedback register can solve that problem

I generated the signal as given in the Fig 130.Quadrature Encoder Basic Operation of UM10360
i am using only 2 signal Pha and Phb
0 件の賞賛
返信

1,649件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Mar 12 12:37:07 MST 2015
Hi Praveen,

There is an Application note on using Motor control in LPC17xx.
http://www.lpcware.com/content/nxpfile/an10898-bldc-motor-control-lpc1700

Thanks,
NXp Technical Support
0 件の賞賛
返信