using a silabs usb debug adapter with LPC1111 and Xpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using a silabs usb debug adapter with LPC1111 and Xpresso

1,019 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by corwinb on Thu Mar 14 13:13:14 MST 2013
I don't see why this cannot be done, after all both adapters must be CoreSight compatable.
When I try to launch the debugger in Xpresso I get the "No emulator/board available" dialog.
I am sure there is some tool setting that I need to change, however, it is not obvious to me.
I am sure some of you folks have pondered this before, and some have likely done it.
Please share.

Thank you.
标签 (1)
0 项奖励
回复
2 回复数

1,008 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by corwinb on Fri Mar 15 11:09:52 MST 2013
Thank you.
0 项奖励
回复

1,009 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Fri Mar 15 00:28:55 MST 2013
Hi corwinb,

Sorry to have to dissapoint you; LPCXpresso does not support the silabs USB debugger. Red Suite (Full License) does support the Silabs debugger (see http://code-red-tech.com/RedSuite5/red-suite-5.php), but I'm not sure if the silabs debugger works with the NXP parts though.

If you want to know more on Red Suite, please contact Code Red since they provide support for their IDE.

Regards,
Wouter
0 项奖励
回复