use SPIFI flash debug code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use SPIFI flash debug code

1,471 Views
dh0219
Contributor I

LPC4330+W25q64

202454g06cfpf90f6ia4mc.png

what’s the matter with my program

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,364 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please provide a little more information about your issue?

Which example are you running? Are you using a NXP board?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply