use SPIFI flash debug code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use SPIFI flash debug code

1,384件の閲覧回数
dh0219
Contributor I

LPC4330+W25q64

202454g06cfpf90f6ia4mc.png

what’s the matter with my program

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,277件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Could you please provide a little more information about your issue?

Which example are you running? Are you using a NXP board?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信