usbhid in lpc1769 requires some delay between the 2 64 bytes interrupt transfers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usbhid in lpc1769 requires some delay between the 2 64 bytes interrupt transfers

918 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sudee on Mon Jan 20 04:32:44 MST 2014
hello.

i am using the lpc1769 running at 120mhz to use it as an hid device with INTERRUPT end point for IN and OUT POINTS with 1msec and 64bytes transfer

, BUT i am facing one problem there i am unable to send multiple 64bytes frames at a time, i need to give some delay in between every frame

transmission this will affect the purpose of my project as i need to collect adc data with specified samples and frequency but for every time i need to

change the delay values

Do you know any clue about delay as the device should send all the data work without delay

ex:
for(i=0;i<5;i++0)
{
usbwriteEP(0x81,64);
Delay(15000);//why i need this
Delay(16000);
}

regards
标签 (1)
0 项奖励
回复
0 回复数