usbd_lib_cdc LPCXpresso 1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usbd_lib_cdc LPCXpresso 1769

1,010 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Sun Jun 22 16:27:44 MST 2014
LPC Open v2.10/LPCXpresso v7.2.0/Windows 7/64

Has anyone had success connecting the USB with usbd_lib_cdc built on the Xpresso Base Board?

If so, will you please share the details/changes/file.inf etc.

Also, I have a question about the underlying library usbd_175x_6x_lib: is there any reason that this library would not support an alternate build for the Code Red RDB1768R2 Development Board?

Thanks!
标签 (1)
0 项奖励
回复
1 回复

990 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Mon Jun 23 13:06:08 MST 2014
Posted this to the wrong forum.

Moved this to the LPC Xpress forum, and posted resolution.
0 项奖励
回复