usb driver for windows10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb driver for windows10

1,980件の閲覧回数
1029124854
Contributor I

LPC2148 usb  driver for windows10.

0 件の賞賛
返信
1 返信

1,755件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Jackie,

The LPC21xx is part of the legacy devices and it has limited support. If you are referring to the USB drivers related to the debugger, you could contact to board manufacturer to ask of there is an updated version. Otherwise, you may consider using an external debugger with updated drivers, like Segger J-Link.

If you refer to custom USB drivers from a programmed USB application on the MCU, I’m afraid that we don’t have, although some of the generic USB drivers (like HID, MSD, CDC) are usually included on the newer operating system, just requiring some modification on the USB descriptors.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信